Skip to main content
Mark Reds
Associate II
October 22, 2019
Question

Debugger not working after upgrade to STM32CubeIDE 1.1.0

Hi,

after upgrading my STM32CubeIDE application to latest version 1.1.0 I'm unable to debug my project.

According to the log it seems that debugger is unable to identify my STM32F401RE anymore.

I tried with a new empty project and I encountered the same issue. Here following the output of the log:

 
STMicroelectronics ST-LINK GDB server. Version 5.3.2
Copyright (c) 2019, STMicroelectronics. All rights reserved.
 
Starting server with the following options:
 Persistent Mode : Disabled
 Logging Level : 1
 Listen Port Number : 61234
 Status Refresh Delay : 15s
 Verbose Mode : Disabled
 SWD Debug : Enabled
 
Waiting for debugger connection...
Debugger connected
 -------------------------------------------------------------------
 STM32CubeProgrammer v2.2.0 
 -------------------------------------------------------------------
 
 
 
Log output file: /tmp/STM32CubeProgrammer_7uowht.log
ST-LINK SN : 50FF71067788545428432167
ST-LINK FW : V2J34S7
Voltage : 3.19V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Cannot identify the device
Error: unknown or unsupported device (DevID = 0x0000)
 
 
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_V9fWXA.srec
 File : ST-LINK_GDB_server_V9fWXA.srec
 Size : 7328 Bytes
 Address : 0x08000000 
 
 
Erasing memory corresponding to segment 0:
Download in Progress:
 
 
File download complete
Time elapsed during download operation: 00:00:00.056
 
 
 
Verifying ...
 
 
 
 
Error: Data mismatch found at address 0x08000004 (byte = 0x55 instead of 0xB1)
 
 
Error: Download verification failed
 
 
Encountered Error when opening /Applications/STM32CubeIDE.app/Contents/Eclipse/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.macos64_1.1.0.201910081157/tools/bin/STM32_Programmer_CLI
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...

This topic has been closed for replies.

11 replies

Massimiliano Galanti
Associate
October 23, 2019

same here with STM32F405RGT6.

-- EDIT --

looking at the release note:

> ST-LINK GDB-server does not work properly with the macOS® version of STM32CubeIDE. The use of OpenOCD or J-Link is required.

-- EDIT SOLVED! --

installed openocd:

brew install openocd

then in IDE:

Debug Configurations -> Debug -> Debug Probe to ST-LINK (OpenOCD)

had also to enable sw reset:

Show generator options... -> Reset Mode -> Software system reset

looks everything is now working as expected!

Mark Reds
Mark RedsAuthor
Associate II
October 24, 2019

It works now, following the suggestion of Massimiliano. Thank you.

mmalex
Associate II
October 25, 2019

thankyou for this solution! I would not recommend upgrading from 1.0.1 to 1.1 for mac users - it's been a frustrating evening!

  • first, the ide hangs when you import your old projects from 1.0.1. This is mentioned in the release notes, but no workaround. so I rebuilt my project by hand
  • then, it fails to flash the board when you hit debug...

so I reinstalled STM32CubeIDE fresh. My mac refused to open the .app saying it was 'damaged, move to trash?'. The fix was (after googling) to run sudo xattr -cr /Applications/STM32CubeIDE.app and this allowed the freshly installed IDE to start

  • but we still have the flash problem... back to google, and we find this answer! thanks to this answer above there is a workaround!

I have a working board again, but I think these issues make the experience of upgrading or installing 1.1 a bit of a pain. I'm mostly writing this in case anyone experiences any of those same issues.

Looking forward to the next patch of the ide. thanks for the awesome platform, despite its mac-y release issues.

charlieAngele
Visitor II
November 3, 2019

Thank you ! I was just doing the "step-by-step" pdf and didn't't understand why the debug wasn't working, think I will install previous version instead.

fred bar
Senior
October 25, 2019

Incredible they let the product out with such problems. Not professional at all.

Mark Reds
Mark RedsAuthor
Associate II
October 25, 2019

I think STM32CubeIDE is a great "all-in-one" tool to start developing your application upon the STM32 platform, but it is still "too young" and need to grow its stability. I hope this will happen in the next releases.

Another bug I found is this version is that seems it is unable to recognise my sources directory is under SVN versioning so the "Team" submenu in the project popup doesn't show anymore all SVN-related commands. For now I will use the command line to commit my changes.

fred bar
Senior
October 25, 2019

The tools are based on very much mature tools and standards. What happened on this release looks like a huge lack of quality testing. Might be planned and intentional, don't know, i certainly do not intend that they lack competence. All they did needs pretty good stack of capabilities.

Most problems are regressions, not youngness problems. Releasing with such a list of known problems and without clearly telling users before updating is very bad practice.

Mark Reds
Mark RedsAuthor
Associate II
October 25, 2019

STM32CubeIDE is "Eclipse IDE", and the Cube is built as a plugin inside the Eclipse IDE, this last one is a mature tool (even I don't like it very much, I always preferred Netbeans, but this is another story...) not the Cube, but this is my personal experience only. Anyway STM32CubeIDE should be tested a bit deeper before published as a new update.

fred bar
Senior
October 25, 2019

So it looks like we agree. (and also on he netbeans part.. microchip made a better move on that, even if netbeans's C editor is a bit lacking)

BDurs
Associate
October 28, 2019

I experience the same problem. I use Windows 10.

Debug via built-in to the Discovery board ST-LINK stopped working. Advices on the forum didn't help. I press "Debug" and nothing happends, literally nothing - no message (even the shortest one), no log, no perspective change, nothing. Until the problem is solved I go back to 1.0.2. I hope it will help.

MHHH.1
Visitor II
January 29, 2020

29 Jan 2020: I've had a VERY SIMILAR experience: I've been using STM32CubeIDE alongside the separate STM32CubeProgrammer for a couple of months. I'm using BluePills (STM32F103) with the ST-LINK V2 JTAG/SWD programmer / ICE.

All the Edit-and-Compile territory seems to work fine, the programmer is on the button, and I've managed to educate myself about the suite while writing / compiling / burning and running several test programs. I gather this tool was previously TrueStudio by Atollic (is that correct ?) and that ST acquired them to build this "in-house" suite.

So far so good. Getting DEBUG to behave took a while -- the ST-LINK I have is fine, never seems to cause issue --- but the full STLINK-with-GDBServer experience I found fails instantly when the GDB server insists on checking the "ID" on the STM32 chip on the board -- this differs by one digit on the BluePills from the supposed ID code - and the GDB server will have no more of it and exits. BUT, up to now - the second option -- "ST-LINK OpenOCD" -- worked FINE, as that check appeared not to be made, and the whole step-through-code / stop and review memory content process, all worked fine, I was even starting to learn some GDB commands, as you get a GDB console still (not quite clear how / this is some alternate incarnation of the GDB service presumably, not made clear in the docs). All of that WORKED FINE all yesterday until..... suddently it didn't. Now, NOTHING: No debug functionality at all: IDE behaves exactly as before, except, when I hit the final "Debug" button in the Debug_Configuration options panel, which previously launched two consoles, one STLINK and one GDB and set off the whole debug cycle....

- ABSOLUTELY NOTHING happens - as if I had not touched the mouse.  

So --- dug around looking at configs, could find nothing relevant.   Ran a  ps -ef | grep gdb   and could see no GDB server running....  even if I switch back to the "ST LINK - GDB Server" option for debug.  Something's not getting launched.  

Battled with this for an hour / finally UNINSTALLED the whole STM32CubeIDE in toto using synaptic:   REINSTALLED, all the way from the downloaded master script.

IDE back up..  EXACTLY THE SAME.  NO Debug functionality at all.     Test the ST LINK with CubeProgrammer --- works fine.  

ST --- this is BRAND NEW V 1.2.0 IDE ST: downloaded clean and new a few days back (was using 1.0.2 before).  What's going on ?  

I thought this code was mature ?

Now I'm reading up on OpenOCD to learn if I can do all this OUTSIDE your IDE.  

Might email this in to ST as well as the community to see what's afoot.  I have WORK to do ST:  tools should just work.   I've put my trust in you -- waiting to buy silicon for products -- can you sort this out please ?