Skip to main content
Associate
Nov 30, 2025 3:39 PM UTC
Solved

Debugger giving an error after uploading code

Nucleo Board STM32F401RE , STM32CubeIDE 1.19 

16x2 LCD confirmed to be working using Arduino Uno

Hi, I am just starting with STM32 and trying to figure out my way around it after using Arduino Uno for a long time for simple projects with sensors. I installed IDE , created a new project, selected my board from the first menu and so far everything is OK. I generated code without changing anything related to clock or the pin out. The problem is that even though I have not added any code to the project, the IDE opens a different c file every time I upload code, sometimes with a HAL in the name other times it opens this file startup_stm32f401xe.s and highlights this line 

ldr sp, =_estack /* set stack pointer */

I went back and enabled the builtin green LED and added 2 lines in the while to toggle it every 500ms, then uploaded the code but weirdly even after the upload is finished sometimes the LED would start toggling on and off but on the next upload it wouldn`t. the exact same code sometimes works and sometimes it doesn`t , while opening the one of the files I mentioned earlier. I tried connecting a16x2 LCD but failed to make it print anything other than empty boxes on the first line of the screen. 

any help is greatly appreciated. 

TDK
TDKBest answer
Nov 30, 2025 7:02 PM UTC

STM32CubeIDE opens a random file each time you launch the debugger. That is a known issue that has been around for years.

"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

TDK
TDKBest answer
Nov 30, 2025 7:02 PM UTC

STM32CubeIDE opens a random file each time you launch the debugger. That is a known issue that has been around for years.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate
Nov 30, 2025 7:06 PM UTC

Yeah I discovered this after lots of googling , I though it was a problem with the whatever that is highlighted by the IDE in the file it opens :( not cool for an stm32 noob