Skip to main content
marco.erni
Associate
January 20, 2020
Question

Debug Start Up Script Comments and Variables

Dear all

I moved from Atollic to Cube IDE.

To debug a firmware without boot loader I use the Run Commands (located in the Debug Configuration -> Startup Tap) to move the $pc (program counter) to the desired address, where the firmware actually starts. This works in Cube IDE as well. But my comments in the same field beginning with a # do not work anymore. When I start the debugging session, I receive the following message:

Failed to execute MI command:

#comment

Error message from debugger back end:

Undefined command: "". Try "help".

1) How can I add comments to my StartUp Run Commands?

At the moment I use a constant number in the StartUp Script to set my program counter. In my source code is a pre-processor define with the actual program counter address.

2) Is there a way to use defines located in the source code in Debug Startup scripts?

I am using ST-Link V2 and CubeIDE 1.2.0 for debugging a STM32F0 MCU.

Thank you for your help.

Marco

This topic has been closed for replies.

1 reply

Pavel A.
January 20, 2020

2) Is there a way to use defines located in the source code in Debug Startup scripts?

Not in source, of course, but maybe the script could allow using Eclipse build variables

-- pa