Skip to main content
koster
Associate II
March 4, 2020
Question

Debug problem after update of STM32CubeIDE from 1.0.2 to 1.2 / 1.3

After update of STM32CubeIDE from 1.0.2 to 1.2 or 1.3 (or installing from the scratch with uninstall before) I can't run the debugger any more. I do not get any output or information in the Debug or Console window. I tried to use H7 with ST-Link and F4 with Segger J-Link, both with the same result.

This topic has been closed for replies.

6 replies

Markus GIRDLAND
ST Employee
March 4, 2020

What happens when you press the debug button? Nothing at all? Is it with a specific project or with every project, even new ones?

Any way you can share about how to reproduce the problem?

koster
kosterAuthor
Associate II
March 4, 2020

Nothing at all, just a very brief flickering in the bottom right corner of the window, but just once after the initial start of the IDE and the first debug trial. I tried this with 2 of my projects (H7 (ST-Link) and F4 (J-Link)), but also with a project generated from scratch with the STM32 Project generator (H7 (ST_Link)).

Markus GIRDLAND
ST Employee
March 5, 2020

While using an ST-Link you can go into the debug configuration and enable a GDB server log in the Debugger tab. Does that have any information in it and if so can you paste it here? Also, if you go to Window -> Preferences -> C/C++ -> Debug -> GDB -> and tick the "Show the GDB traces consoles with character limit". After that you try another debug session and then generate that log as well, might give some clue about what is happening.

GIkar
Associate III
March 4, 2020

My SDIO SD mount doesn't work since the update.

koster
kosterAuthor
Associate II
March 5, 2020

Hi Marcus, I ticked this option and have 2 effects:

  • pressing the bug button, a window pops up and immediately disappears. I just can read 'executable' but not the text before.
  • selecting from the menu (small arrow left of the bug button): a window in the Console area comes and goes, but I can't read anything
koster
kosterAuthor
Associate II
March 17, 2020

any proposals?