Skip to main content
Associate
July 15, 2024
Question

Debug NUCLEO-L552ZE-Q

How can I download my application onto board when debugging from the Cube IDE 1.16 ?

I have the NUCLEO-L552ZE-Q, and using the Cube programmer I can program the .elf to flash as it seems, which takes like 30 seconds.

When I debug from the Cube IDE 1.16 it takes very short time and I see no dowloading of my .elf. 

How can I download my application automatically when going to debug.

This topic has been closed for replies.

2 replies

Andrew Neil
Super User
July 15, 2024

It should do the download when you press the 'Debug' button, but you're not the first today saying that it doesn't:

https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-doesn-t-flash-target-before-debugging/td-p/697397

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
swenetsAuthor
Associate
July 15, 2024

Thanks Andrew,

It starts working w. 1.15.1.

-sten