Debug Error on Dual Core STM34H747I-DISCO Board
Using Application Note AN5361 and a Online ST Video. I have create a project in STM32CubeIDE for the STM32H747I-Disco Board. As a test of the debugging, I have have both cores simply blinking separate LEDs.
I set up the CM7 debug configuration per AN5361 and did not check "Halt all cores" on Reset. Debugging with the CM7 project, runs the application on the board without issue. I am able to set a break point in the CM7's main.c and step through the code. If I set a break point in CM4's main.c, nothing happens. The CM4 is not loaded in the debugger at all.
The online video made the suggestion to check "Halt all cores" on Reset ion the CM7's debug configuration. I created a Launch Group to start debug both projects. Starting debug starts up both projects as expected. The debugger stops at the CM7 main break point. Click continue, and the debugger stops at the CM4 main break point at the line for:
__HAL_RCC_HSEM_CLK_ENABLE();
If I click continue, the program crashes into an unknown space.

If I uncheck the "Halt on cores", and attempt to Debug with the Launch Group fails on the CM4 with a "Failed to Launch GDB Server"
What am I missing? What needs to be configured to debug both projects?