Skip to main content
Associate
Jan 29, 2026 12:40 PM UTC
Question

.d:1: *** multiple target patterns. Stop.

From cube 1.3.0 I always get this error and the cause seems to be the path generation in .d files. In cube 1.12.1 the path is relative but from cube 1.3.0 it is absolute and generates something like \\?\C:\.... So the only solution for me is to stay with cube 1.12.0. The build however seems ok an the bin file is generated. Did anyone had a similar issue? The issue is present only on windows and it seems ok on linux.


arm-none-eabi-size STM32F769I_TEST.elf
arm-none-eabi-objdump -h -S STM32F769I_TEST.elf > "STM32F769I_TEST.list"
arm-none-eabi-objcopy -O ihex STM32F769I_TEST.elf "STM32F769I_TEST.hex"
arm-none-eabi-objcopy -O binary STM32F769I_TEST.elf "STM32F769I_TEST.bin"
text data bss dec hex filename
1227608 43680 452264 1723552 1a4ca0 STM32F769I_TEST.elf
Finished building: default.size.stdout

Finished building: STM32F769I_TEST.hex
Finished building: STM32F769I_TEST.bin


Finished building: STM32F769I_TEST.list

test/web/unicabminnow.d:1: *** multiple target patterns. Stop.
make: *** [makefile:152: all] Error 2
"make -j8 all" terminated with exit code 2. Build might be incomplete.

12:23:07 Build Failed. 3 errors, 408 warnings. (took 1m:27s.726ms)

5 replies

ST Technical Moderator
Jan 29, 2026 1:11 PM UTC

Hello @aljo666 

Let me thank you for posting.

I recommend that you use the last version STM32CubeIDE 2.0.

STM32CubeIDE | Software - STMicroelectronics

Thanks.

Mahmoud

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
aljo666Author
Associate
Jan 29, 2026 1:13 PM UTC

Already tired and the issue is still present.

ST Technical Moderator
Jan 29, 2026 1:21 PM UTC

Could you provide please your STM32CubeIDE Project.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
aljo666Author
Associate
Jan 29, 2026 2:40 PM UTC

I cannot provide you the project but here is the difference in the .d file for long paths. The main project has links to a basic project and you can see that cube 2.0 generates absolute path and cube 1.2 generates relative paths in .d files which I think throws the error.

stm32 cubeide 2.0.0.0
\\?\C:\Projects\274_Ship_smart_cabin\UNIcabSVN\UNIcab\STM32Cube_FW_F7_V1.15.0\Projects\STM32F769I-Discovery\Applications\Datapan\UNIcab\Src\Datapan\FreeRTOS-Plus\FreeRTOS-IoT-Libraries\abstractions\platform\freertos\include\platform\iot_platform_types_freertos.h \ Datapan/UNIcabWeb/unicabminnow.d:1: *** multiple target patterns. Stop.

stm32 cubeide 1.12.1 ../../../../../../../274_Ship_smart_cabin/UNIcabSVN/UNIcab/STM32Cube_FW_F7_V1.15.0/Projects/STM32F769I-Discovery/Applications/Datapan/UNIcab/Src/Datapan/FreeRTOS-Plus/FreeRTOS-IoT-Libraries/abstractions/platform/freertos/include/platform/iot_platform_types_freertos.h \ build ok