Skip to main content
Associate II
Sep 16, 2025 9:28 AM UTC
Solved

CubeMX Generates Incorrect DMA Link in HAL_XSPI_MspInit Function

Bug Report: CubeMX Code Generation Error - Incorrect DMA Link in HAL_XSPI_MspInit Function

 

  1. Environment

 

The software environment is STM32CubeIDE

Version: 1.19.0 Build: 25607_20250703_0907 (UTC)

and the FW used is STM32CubeH7RS Firmware Package V1.2.0 / 05-February-2025.

 

  1. Problem Description

 

When CubeMX generates the

HAL_XSPI_MspInit

function, it incorrectly links

handle_HPDMA1_Channel0

, which is the transmit (TX) DMA channel, to the receive (RX) pointer

hdmarx

of the XSPI handle. This causes manually modified code to be overwritten with the incorrect code every time the

.ioc

file is saved and the code is regenerated.

  • Incorrectly Generated Code:
    __HAL_LINKDMA(hxspi, hdmarx, handle_HPDMA1_Channel0);
  • Correct Code:
    __HAL_LINKDMA(hxspi, hdmatx, handle_HPDMA1_Channel0);
  1. Cause

 

There is an error in the CubeMX code generation logic that incorrectly links the TX DMA channel to the RX pointer within the

HAL_XSPI_MspInit

function.

 

  1. Solution

 

Utilize

USER CODE

blocks to protect manual modifications. By placing the correct code within

USER CODE

blocks, CubeMX will not overwrite the contents of these blocks during code regeneration.

 

Cleanest Modification Method:

  1. Open the
    stm32h7rsxx_hal_msp.c
    file.
  2. Find the
    hxspi->Instance==XSPI2
    block within the
    HAL_XSPI_MspInit
    function.

Leave the code generated by CubeMX as is, and add the following correct link code inside the

/* USER CODE BEGIN XSPI2_MspInit 1 */
block:
/* stm32h7rsxx_hal_msp.c */



void HAL_XSPI_MspInit(XSPI_HandleTypeDef* hxspi)

{

 // ... (XSPI2 MspInit top part code) ...



 else if(hxspi->Instance==XSPI2)

 {

 /* USER CODE BEGIN XSPI2_MspInit 0 */

 /* USER CODE END XSPI2_MspInit 0 */



 // ... (CubeMX generated clock, GPIO, DMA Channel 1 (RX) initialization code) ...

 // ...

 __HAL_LINKDMA(hxspi, hdmarx, handle_HPDMA1_Channel1);

 // ...



 // ... (CubeMX generated DMA Channel 0 (TX) initialization code) ...

 if (HAL_DMA_Init(&handle_HPDMA1_Channel0) != HAL_OK)

 {

 Error_Handler();

 }



 // ▼▼▼ CubeMX generated buggy code (leave as is) ▼▼▼

 __HAL_LINKDMA(hxspi, hdmarx, handle_HPDMA1_Channel0);



 if (HAL_DMA_ConfigChannelAttributes(&handle_HPDMA1_Channel0, DMA_CHANNEL_NPRIV) != HAL_OK)

 {

 Error_Handler();

 }



 /* XSPI2 interrupt Init */

 HAL_NVIC_SetPriority(XSPI2_IRQn, 0, 0);

 HAL_NVIC_EnableIRQ(XSPI2_IRQn);



 /* USER CODE BEGIN XSPI2_MspInit 1 */



 /* ==================== Final Solution Code ==================== */

 // Overwrite the incorrectly linked hdmarx with the correct hdmatx.

 // This code will be preserved even upon regeneration.

 __HAL_LINKDMA(hxspi, hdmatx, handle_HPDMA1_Channel0);

 /* ========================================================== */



 /* USER CODE END XSPI2_MspInit 1 */

 }

}

 

This topic has been closed for replies.
Souhaib MAZHOUDBest answer
ST Technical Moderator
Sep 17, 2025 8:39 AM UTC

Hello @YoungKwan 

Actually, you should modify the DMA Handle in IP Structure to hdmatx instead of hdmarx.

SouhaibMAZHOUD_0-1758098269305.png

 

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

4 replies

ST Technical Moderator
Sep 16, 2025 9:38 AM UTC

Hello @YoungKwan 

First let me thank you for posting and welcome to the ST Community.

For more investigation, I suggest that you provide your .IOC file.

Thanks.

Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
YoungKwanAuthor
Associate II
Sep 17, 2025 3:20 AM UTC

I attched IOC file and please investigate it.

Many thanks.
YK

Souhaib MAZHOUDBest answer
ST Technical Moderator
Sep 17, 2025 8:39 AM UTC

Hello @YoungKwan 

Actually, you should modify the DMA Handle in IP Structure to hdmatx instead of hdmarx.

SouhaibMAZHOUD_0-1758098269305.png

 

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
YoungKwanAuthor
Associate II
Sep 17, 2025 3:17 AM UTC

Same problem looks exist at HAL_XSPI_MspDeInit funtion as like below.

Please take look at it .

void HAL_XSPI_MspDeInit(XSPI_HandleTypeDef* hxspi)
{
if(hxspi->Instance==XSPI1)
{
/* USER CODE BEGIN XSPI1_MspDeInit 0 */

/* USER CODE END XSPI1_MspDeInit 0 */
.....

/* XSPI1 DMA DeInit */
HAL_DMA_DeInit(hxspi->hdmarx);
HAL_DMA_DeInit(hxspi->hdmarx);   //<-- Is this correct too? 

/* XSPI1 interrupt DeInit */
HAL_NVIC_DisableIRQ(XSPI1_IRQn);
/* USER CODE BEGIN XSPI1_MspDeInit 1 */

/* USER CODE END XSPI1_MspDeInit 1 */
}
.....
}