Skip to main content
debugging
Lead
May 12, 2024
Solved

CubeMX 6.11.1 & CubeIDE 1.10.1 CMIS_OS2.h OS_TICK.H drivers errors

Building simple project (just enabling UART and XTAL OSC) SMT32F401CCU6 project generates this error.

Have been using STMcubeMX/IDE for years, but never encountered this with the UDE.

MX and IDE have been updated the the latest version

none-eabi-gcc "../Drivers/CMSIS/RTOS2/Source/os_systick.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DDEBUG -DUSE_HAL_DRIVER -DSTM32F401xC -c -I../Core/Inc -I../Drivers/STM32F4xx_HAL_Driver/Inc -I../Drivers/STM32F4xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32F4xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Drivers/CMSIS/RTOS2/Source/os_systick.d" -MT"Drivers/CMSIS/RTOS2/Source/os_systick.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Drivers/CMSIS/RTOS2/Source/os_systick.o"
In file included from ../Drivers/CMSIS/RTOS2/Template/cmsis_os1.c:28:
../Drivers/CMSIS/RTOS2/Template/cmsis_os.h:157:10: fatal error: cmsis_os2.h: No such file or directory
157 | #include "cmsis_os2.h"
| ^~~~~~~~~~~~~
compilation terminated.
../Drivers/CMSIS/RTOS2/Source/os_systick.c:25:10: fatal error: os_tick.h: No such file or directory
25 | #include "os_tick.h"
| ^~~~~~~~~~~
compilation terminated.
make: *** [Drivers/CMSIS/RTOS2/Template/subdir.mk:19: Drivers/CMSIS/RTOS2/Template/cmsis_os1.o] Error 1
make: *** Waiting for unfinished jobs....
make: *** [Drivers/CMSIS/RTOS2/Source/subdir.mk:25: Drivers/CMSIS/RTOS2/Source/os_systick.o] Error 1
"make -j4 all" terminated with exit code 2. Build might be incomplete.

This topic has been closed for replies.
debugging
debuggingBest answer
Lead
May 12, 2024

After installing 1.15 thing went back to normal. The errors disappeared (no code or any changes).... Not sure why...

2 replies

debugging
debuggingAuthor
Lead
May 12, 2024

Hmm CubeIDe seems on version 1.15 now. Always used the update it using the IDE update function but that did not update, so did not notice the latest version

debugging
debuggingAuthorBest answer
Lead
May 12, 2024

After installing 1.15 thing went back to normal. The errors disappeared (no code or any changes).... Not sure why...