Skip to main content
Eqqman
Associate III
March 26, 2024
Solved

CubeIDE running incorrect version of firmware

Using the following version of Cube:

 

Version: 1.14.1

Build: 20064_20240111_1413 (UTC)

 

We first changed the repository location for downloading packages. Then we manually downloaded the U5 package (why is this not available from the package manager?) and installed it. Later we used the package manager to download the F4 support package. The problem we have is that no matter what processor we select for a new project Cube insists on using the U5 package, thus we get errors with all projects we attempt to start on F4 processors. How do you tell Cube which firmware package to use in your project, or how do you change this for existing projects?

This topic has been closed for replies.
Rim LANDOLSI
Rim LANDOLSIBest answer
ST Employee
March 26, 2024

Hello @Eqqman and welcome to the community,

First try checking the proxy settings by following these steps:
- In Window --> Preferences --> Network Connection, enable Native provider.
- Under Window --> Preferences --> Firmware Updater, click on Check Connection
Don't forget to Apply and Close if the connection works.

Then login to "myST" to download new firmware packages.

After creating a project, check that the firmware installation repository is the correct location that you have changed.

Thanks,
Rim.

2 replies

Rim LANDOLSI
Rim LANDOLSIBest answer
ST Employee
March 26, 2024

Hello @Eqqman and welcome to the community,

First try checking the proxy settings by following these steps:
- In Window --> Preferences --> Network Connection, enable Native provider.
- Under Window --> Preferences --> Firmware Updater, click on Check Connection
Don't forget to Apply and Close if the connection works.

Then login to "myST" to download new firmware packages.

After creating a project, check that the firmware installation repository is the correct location that you have changed.

Thanks,
Rim.

Eqqman
EqqmanAuthor
Associate III
March 27, 2024

This seems to have helped, thank you!