Skip to main content
Blem.1
Associate
March 26, 2020
Question

CubeIDE Rendering issues on Linux (SOLVED)

I have some annoying rendering issuse with CubeIDE 1.3 running on Ubuntu 19.10 (Pop_OS).

The problem is that some of the toolbox windows are not updating/re-rendering when switching tabs or perspective.

Debug perspective seems to have most issues, see attached screenshot.

I have tried launching CubeIDE with the following command: "env SWT_GTK3=0 SWT_WEBKIT2=1 /opt/st/stm32cubeide_1.3.0/stm32cubeide %F", and it does not seem to help.

I have an AMD GPU, and are running X11.

Any suggestions?

This topic has been closed for replies.

1 reply

Blem.1
Blem.1Author
Associate
March 26, 2020

I found the answer myself: the POP-OS theme caused the issue. Switched to Adwata and the problems went away.