Skip to main content
Explorer
Aug 8, 2025 8:18 AM UTC
Question

CubeIDE not linking libraries from header files

Hi

I'm building a project from zero and I'm importing all the needed folders manually by going in 

Project -> properties -> C/C++ General -> Path and Symbols -> Add ...

In this way I added all the folder with the needed files. 

Now, when I build the project I have several errors, as an example: "Undefined Reference to UTIL_TIMER_SetPeriod"

However, If I right click on line with error that contains UTIL_TIMER_SetPeriod, the function is correcly showed in its .h file (stm32_timer.h).

The point is:
- I do have included .....Utilities/timer  folder that contains stm32_timer.h file.

- I do have #include "stm32_timer.h" in the .c file that calls the function.

- As I said, if I right click on UTIL_TIMER_SetPeriod and open its declaration, the function is corretly found in its .h file. 

 

This issue is happening with several other functions and TypeDefs that are acuatlly found with right click and its path included.

 

How could I solve this?

Thanks

 

This topic has been closed for replies.

1 reply

TDK
Aug 8, 2025 1:40 PM UTC

Include your code and a screenshot of the error. You're missing something.

Sounds like the UTIL_TIMER_SetPeriod function is not being compiled. Where is that code at?

"If you feel a post has answered your question, please click ""Accept as Solution""."