Skip to main content
Lagodolio
Associate III
March 26, 2021
Question

CubeIDE & FreeRTOS on H743

Hello,

I have a problem with my H7 and FreeRTOS.

I have 3 thread:

/* Definitions for defaultTask */
osThreadId_t defaultTaskHandle;
const osThreadAttr_t defaultTask_attributes = {
 .name = "defaultTask",
 .priority = (osPriority_t) osPriorityAboveNormal,
 .stack_size = 2048 * 4
};
/* Definitions for USB_ReceiveData */
osThreadId_t USB_ReceiveDataHandle;
const osThreadAttr_t USB_ReceiveData_attributes = {
 .name = "USB_ReceiveData",
 .priority = (osPriority_t) osPriorityNormal,
 .stack_size = 832 * 4
};
/* Definitions for ADC_Task */
osThreadId_t ADC_TaskHandle;
const osThreadAttr_t ADC_Task_attributes = {
 .name = "ADC_Task",
 .priority = (osPriority_t) osPriorityBelowNormal,
 .stack_size = 768 * 4
};

and a Semaphore:

/* Definitions for Semaphore_resource */
osMutexId_t Semaphore_resourceHandle;
const osMutexAttr_t Semaphore_resource_attributes = {
 .name = "Semaphore_resource"
};

The first task is for USB & TouchGFX:

void StartDefaultTask(void *argument)
{
 /* init code for USB_DEVICE */
 MX_USB_DEVICE_Init();
 /* USER CODE BEGIN StartDefaultTask */
 MX_TouchGFX_Process();
	/* Infinite loop */
	for(;;)
	{
osSemaphoreAcquire(Semaphore_resourceHandle, 100);
	osSemaphoreRelease(Semaphore_resourceHandle);
		osDelay(1);
	}
 /* USER CODE END StartDefaultTask */
}

The second one receives commands from pc and moves a servomotor:

void USB_Receive_Data(void *argument)
{
 /* USER CODE BEGIN USB_Receive_Data */
	/* Infinite loop */
	
	for(;;)
	{
		
		if ((VCP_chkInputData()==true))
		{
			command actual_command;
			actual_command=	VCP_retrieveInputData();
			command_to_motor(actual_command);
		}
		
		osDelay(5);
	}
 /* USER CODE END USB_Receive_Data */
}

Sending command to servo can take 20ms.

And finally, a task that read from ADC and sends data to PC (data are used by a PID and to show info)

void Start_ADC_Task(void *argument)
{
 /* USER CODE BEGIN Start_ADC_Task */
 
 
	/* Infinite loop */
	for(;;)
	{
	
		/****************************************
			 READ DATA	 
		 ****************************************/
		osSemaphoreAcquire(Semaphore_resourceHandle, 100);
 
 
			Read_CH23(); read channel 1-2
			Read_CH45(); read channel 3-4
 
 
			uint8_t valiex;
 
			valiex=	CDC_Transmit_FS((uint8_t*)united_data.buffer_csv, sizeof(united_data.buffer_csv));
			if (valiex==USBD_OK)
			{
				MOTOR_MOV_NOT_ALLOWED=false;
				error_counter=0;
			}
			else{
				error_counter++;
				if (error_counter>15)
				{
				error_counter=0;
				error_USB();
 
				}
			}
#endif
		}
		osSemaphoreRelease(Semaphore_resourceHandle);
 
osDelay(1);
	}
}

If I read @30Hz, I have no problem, but if I increase the sampling rate to @150 the tasks break down...

Sometimes it doesn't accept commands from USB, other times stop sending data from ADC.

I tried to increase/decrease osDelay () and task priority but without results.

Any idea?

Thanks and best regards

This topic has been closed for replies.

1 reply

Lagodolio
LagodolioAuthor
Associate III
March 29, 2021

I think the problem is in the osDelay() values (do I need to increase them?) but I'm not sure how to define these delays: I set TouchGFX to osDelay(100) without problems but between ADC function (about 5-6 ms to complete the function) and USB to motor (from 0 -no instruction- to 50ms) all is more complicated.

"USB_Receive_Data" receives data from USB and sends it to the motor via MODBUS, and every message needs about 10ms of delay. These delays are via vTaskDelay(), so i.e. Start_ADC_Task() can use this time to give me a value.

Sometimes, the system slows down in data exchange responsiveness. I tried to use Percepio Tracealyzer but I have an SWD interface and it seems not to permit live analysis. Can someone suggest me a method for tuning my FREERTOS?

Thanks!