Skip to main content
Pavel A.
February 15, 2021
Question

CubeIDE, failure to import existing project

I've imported a SW4STM example into CubeIDE, it worked fine.

Then I import this already converted project into another CubeIDE workspace and this fails.

The project becomes "orphaned", no toolchain defined.

It looks like CubeIDE creates duplicate Debug config. After import there's two configurations named Debug.

I deleted one and the 'orphaned' error disappeared. But the project still does not build, something is broken. :(

CubeIDE version 1.5.1 on Ubuntu, target MCU is STM32H743

-- pa

This topic has been closed for replies.

5 replies

Markus GIRDLAND
ST Employee
February 16, 2021

Just so I get a clear understanding of the issue:

  1. You import an SW4STM32 example into an older version of CubeIDE to then import to a newer one? Or from 1.5.1 to another workspace still being 1.5.1?
  2. How do you import the project from one CubeIDE to the other? (Or the other workspace with the same version if that's the case)
  3. Which example did you use? I have access to a Ubuntu machine so I could try to reproduce the problem.
Pavel A.
Pavel A.Author
February 16, 2021

Hi Markus, thanks for your attention

  1. Recent CubeIDE: 1.5.1 , imported an example from Cube package for H7
  2. Import existing project into workspace, with the same CubeIDE.
  3. Example is GPIO_EXTI

-- pa

Markus GIRDLAND
ST Employee
February 17, 2021

Hello again!

I tried this with the GPIO_EXTI example located at C:\Users\userName\STM32Cube\Repository\STM32Cube_FW_H7_V1.6.0\Projects\NUCLEO-H743ZI\Examples\GPIO\GPIO_EXTI using STM32CubeIDE 1.5.1 but I wasn't able to reproduce the behavior.

These were my steps:

  1. Using workspace 1.5.1 I used Import -> ac6 project -> selecting the GPIO_EXTI folder.
  2. Project imports, converts and builds successfully
  3. Using workspace 1.5.1_2 I used Import -> Existing project into workspace -> selecting the GPIO_EXTI folder
  4. Project imports and builds successfully.

Do you move the project at all for use in "workspace 2" or copy it to a new location? The firmware packages have a lot of references inside the firmware package structure that requires the package to be consistent in its structure.

Did you close STM32CubeIDE after step 2 in my list above?

If I'm missing some step or misunderstanding then please let me know!

Pavel A.
Pavel A.Author
February 18, 2021

Hi Markus,

The 2nd time I don't select "copy project into workspace".

I'd like it to stay in the original place with all its dependencies.

The problem is not that it won't build successfully after 2nd import, but that it even loses some basic features (natures or whatever)

-- pa