Skip to main content
Senior
September 9, 2024
Question

CubeIDE does not update touchgfx display

Any project I have tried to run from the CubeIDE will only display a static screen. I am using the STM32H7B3I-DK.
I currently have my project setup to show one screen for a second and then switch to another that has wildcard values that update. The screen  switch will occur, but the wildcard values stay as their SetupScreen() value. The screen then doesn't take any input. 
I have gotten it to run properly by using the Program and Run Target button that is in the touchgfx designer, but with that I had to copy and paste all my custom source and include files into the core dir as the include paths weren't working when I added them to the makefile.

I know these are two separate issues, so I would like to just tackle getting the CubeIDE running my project properly for now.


This topic has been closed for replies.