Skip to main content
spica lai
Associate II
April 14, 2020
Question

cubeide can not choose firmware package

hi, I am using cubeide v1.3 on win10.

While I am trying to generate code automatically using cubeide, I found I cannot change the firmware package name and version.

Since I only installed STM32CubeFW_F4 V1.24.0, and I donot wanna update to the newest version which is 1.25. How can I change the setting, which now is not editable.

This topic has been closed for replies.

9 replies

Cartu38 OpenDev
Graduate II
April 14, 2020

Not possible. Or at least not possible if creating a new ​project. STM32Cube ecosystem is forcing you to use most recent version of firmware pack.

If having already an existing project then even if updating STM32Cube tool suite former versions of pack​ (the one your project is based on) is supported.

Nesrine.JLASSI
Visitor II
April 14, 2020

Hi @spica lai​ 

STM32CubeIDE forces the user to use the most recent version of the firmware.

Regards,

Nesrine

spica lai
spica laiAuthor
Associate II
April 15, 2020

thx a lot.

​

However, I found a way to resolve this by edit *.ioc using an external text editor like this:

ProjectManager.FirmwarePackage=STM32Cube FW_F4 V1.24.0

​

which is quite arbitory.

​

Anyway, It is better to let users change it in a more convenient way.

Nesrine.JLASSI
Visitor II
April 15, 2020

Hello @spica lai​ 

Thanks for your feedback, the reported problem has been detected and will be reviewed by STM32CubeIDE team.

I'll get back to you if there's any news.

Best regards,

Nesrine

spica lai
spica laiAuthor
Associate II
April 15, 2020

BTW, I found a bug of CubeIDE.

When I didnot connect internet and start CubeIDE (open CubeIDE before internet is connected), I failed to open Embedded Software Package Manager.

The detail is:

  1. Start CubeIDE.
  2. Click Help->Embedded Software Package Manager.
  3. It cames out a dialog as attachment.
  4. If I choose yes, it comes out some settings of CubeIDE.
  5. If I choose no, nothing happened.

As a whole, if I was offline, the Embedded Software Package manager cannot be opened.

That is to say, the package can not be installed from local OFFLINE.

Nesrine.JLASSI
Visitor II
April 15, 2020

Okay, i will check this then i'll get back to you.

Regards,

Nesrine

Nesrine.JLASSI
Visitor II
April 15, 2020

Hello @spica lai​ 

You have to do this following step:

  1. Start CubeIDE.
  2. Click Help the select Manage Embedded Software Packages .
  3. It cames out a dialog .
  4. Choose yes ==>  it comes out some settings of CubeIDE
  5. Please apply off line Mode as attachment.0693W000000VrshQAC.png
  6. Click Apply and Close

Best regards,

Nesrine

spica lai
spica laiAuthor
Associate II
April 16, 2020

thx a lot for your reply.

I have done want you have said.

however, when I clicked Embedded Software Package Manager again, nothing came out. The manager dialog doesnot come out.

Here is my experement:

  1. If always offline (not connected internet before open cubeide), no manager comes out.
  2. If connected internet and open cubeide and keep online, manager comes out.
Nesrine.JLASSI
Visitor II
April 16, 2020

Hi @spica lai​ 

I tested the same scenario: I didn't connect internet then i start CubeIDE (open CubeIDE before internet is connected), I can open Manage Embedded Software Package normally.

Please try to reinstall the CubeIDE, then tell me if the problem still exists.

Best regards,

Nesrine