Skip to main content
ark2
Associate II
Mar 27, 2024 5:27 AM UTC
Question

CUBE IDE No source available for "() at 0xfffffffe" Errors

 

I was making a project with CUBE IDE and compiling it on the board, and I got this error while compiling the project I was doing on the new board.

No source is available for "Call Signal Handler"() in 0xfffffffe.

I'm sure they're using the same CPU

I can't compile it because it's STM32 ST-LINK

I don't think there will be any problems with the code or MX settings because if I modify the code on the existing board, the project will also change well.



Even if I create a new project and add the above code, I get the same error, so I can't compile it

I want to solve this phenomenon, how do I solve it?

 

 

int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MPU Configuration--------------------------------------------------------*/
 MPU_Config();

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 /* USER CODE BEGIN 2 */

 HAL_GPIO_WritePin(GPIOK, GPIO_PIN_2, GPIO_PIN_SET);

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

 

 

The same error occurs in the above simple code.

How can I fix this problem?

 

stm32 : STM32H743XIH6

==========================================

Error image

01.JPG

=========================================
Current state

00.JPG

 

01.JPG

 

02.JPG

 

03.JPG

 

 

 

2 replies

Andrew Neil
Super User
Apr 3, 2024 9:20 AM UTC

0xfffffffe is a "magic" address in the ARM Cortex-M architecture which indicates a core lockup; eg, a double Hardfault:

https://forum.microchip.com/s/topic/a5C3l000000UjLaEAK/t187425#:~:text=The%20magic%20PC%20value%20of%200xfffffffe%20indicates%20core%20lock%2Dup.%20This%20generally%20happens%20when%20the%20CPU%20double%2Dhardfaults.%20For%20example%2C%20a%20CPU%20hardfault%20occurs%2C%20and%20another%20fault%20occurs%20while%20trying%20to%20save%20state%20for%20the%20first%20fault%20because%20either%20the%20vector%20table%20is%20bad%2C%20or%20the%20stack%20pointer%20is%20invalid.

https://developer.arm.com/documentation/ddi0403/d/System-Level-Architecture/System-Level-Programmers--Model/ARMv7-M-exception-model/Unrecoverable-exception-cases?lang=en

 


@ark2 wrote:

I was making a project with CUBE IDE and compiling it on the board, and I got this error while compiling the project


Note that this is not an error that you'd get while compiling: this is a runtime error - it means your code is crashing while it's running on your board.

 


@ark2 wrote:
I can't compile it because it's STM32 ST-LINK

That makes no sense. What do you mean by that?

 


@ark2 wrote:
 

Even if I create a new project and add the above code, I get the same error, so I can't compile it


Again, the message has nothing to do with compiling.

Does the code build cleanly - ie, with no errors and no warnings?

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Visitor II
Jan 8, 2026 12:41 PM UTC

Screenshot From 2026-01-08 20-36-27.png

I'm experiencing the same thing.

But mine can execute the code and experience changes in my MCU, such as LED blinking, and there are no error messages at all.

Is this a problem or is that how it works?

What is this usually called?