Skip to main content
WTetl.1
Associate
May 22, 2020
Question

Cube IDE debugger cannot stay connected

I am using a Nucleo-F103RB dev board with Cube IDE 1.3.0. I am able to successfully flash the board (which I have tested by making the user LED on the nucleo toggle at different frequencies), but immediately after this is successful, I lose connection to the debugger. I have the SWD pins enabled and the debug mode set to SWD and so on. Here is what the console prints out:

STMicroelectronics ST-LINK GDB server. Version 5.5.0

Copyright (c) 2019, STMicroelectronics. All rights reserved.

Starting server with the following options:

    Persistent Mode      : Disabled

    Logging Level       : 1

    Listen Port Number     : 61234

    Status Refresh Delay    : 15s

    Verbose Mode        : Disabled

    SWD Debug         : Enabled

    InitWhile         : Enabled

Waiting for debugger connection...

Debugger connected

   -------------------------------------------------------------------

            STM32CubeProgrammer v2.4.0          

   -------------------------------------------------------------------

ST-LINK SN : 066AFF575251717867103959

ST-LINK FW : V2J36M26

Voltage   : 3.27V

SWD freq  : 4000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID  : 0x410

Device name : STM32F101/F102/F103 Medium-density

Flash size : 128 KBytes

Device type : MCU

Device CPU : Cortex-M3

Memory Programming ...

Opening and parsing file: ST-LINK_GDB_server_a13700.srec

 File     : ST-LINK_GDB_server_a13700.srec

 Size     : 12264 Bytes

 Address    : 0x08000000 

Erasing memory corresponding to segment 0:

Erasing internal memory sectors [0 11]

Download in Progress:

File download complete

Time elapsed during download operation: 00:00:01.015

Verifying ...

Download verified successfully 

Debugger connection lost.

Shutting down...

The debugger loses connection immediately after the download is completed. Everything after "Debugger connected" prints at the same time.

If I go to debug mode, it says there is a suspension at HAL_Init(), which cannot be the case because I have confirmed the program is successfully running on the board. I have checked other posts with the same problem and they are not relevant to my question as I have always seen that their solution was already the case for me. I have also attached a screenshot of the debugger tab in Cube, but haven't changed anything from the default settings.

This topic has been closed for replies.

2 replies

SpinKernel
Associate III
May 22, 2020

*don't forget to click debug main.c not run, i was doing that by mistake*

WTetl.1
WTetl.1Author
Associate
May 22, 2020

It was working fine for me a few weeks ago as well. Didn't change anything to my knowledge.