Skip to main content
Tytan28
Associate
Dec 10, 2019 6:35 PM UTC
Question

Cube IDE Compiler error2

Hi,

I'm trying to compile one of AWS project for L475 IoT and I have the silly error:

make[1]: *** [vendors/st/stm32l475_discovery/BSP/B-L475E-IOT01/subdir.mk:39: vendors/st/stm32l475_discovery/BSP/B-L475E-IOT01/stm32l475e_iot01.o] Error 2
 
make: *** [makefile:69: all

Any idea?

Also I will be very happy if anyone will point me to some good manual ;)

This topic has been closed for replies.

3 replies

Pavel A.
Dec 10, 2019 10:22 PM UTC

Have you built this project successfully once, or you're building it first time?

Try to clean the project.

The manual for MAKE is here. Errors: appendix B. (but it isn't too helpful in this case \)

-- pa

Tytan28
Tytan28Author
Associate
Dec 11, 2019 9:35 AM UTC

Hi Pavel,

This is the problem can't compile since beginning. I download source code from amazon then import to my CubeIDE build and I get error.

I was thinking it is problem with folder read only attribute but is not.

K@

Markus GIRDLAND
ST Employee
Dec 11, 2019 1:13 PM UTC

This issue is caused by the include paths having -I in them. For example when B-L475E-IOT01 is mentioned. The -I messes up the include paths (because that is usually the argument for an include path) which is a bug.

Fortunately, this is already fixed in our internal weekly build and will be part of the next release.

If you can't wait for that it might be possible to put all include paths in quotation marks which will most likely solve the problem as well, haven't tested myself.