Skip to main content
Associate II
April 5, 2024
Question

comply a product to get UL certified

Hi 
I am working on a product using STM32H563, which requires to be UL certified.

In-order to make my code comply with UL certification, I am planning to follow the below approach:

  • I am planning to create a spatial separation between critical and non-critical function. by using the TrustZone feature available on the controller
  • I also wanted to use self-test library provided by ST to periodically check heath of CPU,clock,RAM and Flash.
    For this approach I wanted to know whether to use Self test Library as a part of Secure/Critical region.
    What is the good option.
    option-1: STL library as a part of Secure but periodic check from Nonsecure.
    option-2: STL library as a part of Secure and periodic check from secure.

 

 

This topic has been closed for replies.