Skip to main content
Associate III
September 26, 2024
Solved

Compilation error on a file not included in the project

  • September 26, 2024
  • 1 reply
  • 886 views

In my project I use some git submodules to add features.

One of this submodules has a complex folder structure to add documentation, tests, examples and so on. But I only need the src folder.

Given how Git submodules work, the entire folder structure is downloaded, so I had to remove the unwanted folders from the compilation.

Now I can use the submodule and compile my project, but in the test folder of the submodule there is a main.c file that I don't include in my compilation. I tried to write a malformed line of code to see if it would report an error or not and I am sure that that file is not compiled, since I don't get the error.

But I still get an error after the compilation:

 

The float formatting support is not enabled, check your MCU Settings from "Project Properties > C/C++ Build > Settings > Tool Settings", or add manually "-u _printf_float" in linker flags.

 

The error points to the following line in the main.c:

 

 

printf("Coverage : %f\r\n", (float)(tests_passed) / (float)(tests_passed + tests_failed));

 

 

As I said, I'm sure that the file is not compiled, because if it were it would generate a syntax error.

How come it emit an error about the project configuration?

I tried following the error message and enabled the printf checkbox and the error actually goes away, but that's not the way I want to fix this.

This topic has been closed for replies.
Best answer by Douglas MILLER

This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.

1 reply

Douglas MILLER
Douglas MILLERBest answer
ST Employee
September 27, 2024

This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.