Code generation could not be done most probably because the necessary firmware package is missing
Hi
I am using STM32F446ZET6 board but I am unable to generate code. I am facing this issue "Code generation could not be done most probably because the necessary firmware package is missing" I have tried all the process which are mentioned on different platform even on ST community page. I tried to download the firmware package manually and installed it but the error is same. kindly tell me what should I do. STM32CubeIDE version is 1.14.1. and firmware package version is 1.28.0. but nothing is working after every possible solution.