Code built with CubeH7 v1.12.1 fails when loaded by custom bootloader (works fine with v1.12.0)
- 1 reply
- 270 views
Hello ST team,
I’m developing on a STM32H755BITx dual-core (Cortex-M7 / M4) using STM32CubeIDE and STM32CubeH7 HAL.
I have a custom bootloader that starts the user application located at 0x08040000 (M7 app) and 0x08100000 (M4 app).
Context
Bootloader and application are both generated with STM32CubeIDE.
The bootloader runs correctly and can jump to the application.
Everything works fine when the application is compiled using STM32CubeH7 v1.12.0.
But when I rebuild the exact same application using STM32CubeH7 v1.12.1, the app starts but hangs — no LED toggling, no interrupts, no SysTick activity.
Configuration
MCU: STM32H755BITx
IDE: STM32CubeIDE (latest version available)
Bootloader base M7: 0x08000000
- Bootloader base M4: 0x08020000
App M7 base: 0x08040000
App M4 base: 0x08100000
Dual-core synchronized via HSEM
Power configuration macro used: USE_PWR_LDO_SUPPLY
Symptoms
When jumping to the app built with v1.12.1:
The vector table and MSP are correct (checked with debugger).
The app reaches main(), but HAL_Delay() and all IRQ-based functions stop working.
LEDs never toggle.
SysTick and TIM interrupts appear inactive.
The exact same binary rebuilt with v1.12.0 works perfectly.
ATTACHED MAIN.C OF THE BOOTLOADERS.
Could you please:
1) Confirm if there are known issues in STM32CubeH7 v1.12.1 affecting SysTick or RCC initialization?
2) Suggest the recommended workaround or patch for applications started by a custom bootloader.
Thank you very much for your support!
Best regards!