CMSIS pack DSP libraries aren't being stitched into projects
STM32CubeIDE 1.14.0
STM32H563ZI Nucleo board
In <Software Packs> <Manage Software Packs><ARM> install CMSIS 5.6.0
In <Software Packs><Select Components> and select <CMSIS DSP> 1.7.0 <Library> and hit OK
So, this should do "The Right Thing", except it doesn't actually pull the proper .lib or .a or ??? out of the pack and stitch it into the project in <Drivers><CMSIS><should be Library>. Bummer.
For this processor there are 5 candidate libraries available, all I know is that I have a arm8m, so:
arm_ARMv8MBLl_math.lib
arm_ARMv8MMLl_math.lib
arm_ARMv8MMLld_math.lib
arm_ARMv8MMLldfsp_math.lib
arm_ARMv8MMLlfsp_math.lib
Any chance that, in the future, the .lib or .a file be copied into the project and the appropriate gcc flags get thrown to find the file?
In the mean time, any idea which .lib/.a file is appropriate for an H563?
Thanks,
Andrei (from The Great White North)