Skip to main content
SKim.2344
Associate
Dec 9, 2019 12:55 AM UTC
Question

Cme.exe and WMIC.exe Processors Continue to Generate When Running CubeIDE 1.1.0

I have a question about running CubeIDE.

I used CubeIDE 1.0.2 and then upgraded to CubeIDE 1.1.0.

The problem is that when I run CubeIDE 1.1.0 the cme.exe and WMIC.exe processors continue to be generated.

If I exit CubeIDE 1.1.0, all cme.exe and WMIC.exe that were created will also be shut down.

How can I solve this problem?

The same problem occurs when I uninstall CubeIDE 1.0.2 and install CubeIDE 1.1.0.

I am using win7 64-bit.

This topic has been closed for replies.