Skip to main content
Senior III
Mar 27, 2025 11:49 AM UTC
Solved

Cant import a project into a workspace

STM32CubeIDE 1.17.0, Win 11 x64

I have a number of related projects in the space workspace (WS). I can copy & paste them into the same WS with no problem within CubeIDE. New project folders are created within the WS directory & show up in the Project Manager list. All these project folders exist within the WS directory.

When I import a project from outside the WS using Open Projects from File System... they import fine & show up in the Project Manager list.

 

BUT when I try to cut & paste a project folder from outside of the WS directory into the WS directory via Windows Explorer & then try an add it to the Project Manager list in CubeIDE via Open Projects from File System... I get nothing, no import error messages, nothing. The project file doesn't appear in the Project Manager list, nothing!

Anyone know why this is?


This topic has been closed for replies.
Pavel A.
Pavel A.Best answer
Mar 28, 2025 12:48 AM UTC

> BUT when I try to cut & paste a project folder from outside of the WS directory into the WS directory via Windows Explorer & then try an add it to the Project Manager list in CubeIDE via Open Projects from File System.

Correct way is: File... Import... Existing project into Workspace.

 

1 reply

Pavel A.
Pavel A.Best answer
Mar 28, 2025 12:48 AM UTC

> BUT when I try to cut & paste a project folder from outside of the WS directory into the WS directory via Windows Explorer & then try an add it to the Project Manager list in CubeIDE via Open Projects from File System.

Correct way is: File... Import... Existing project into Workspace.