Cannot install stm32cube_fw_f4_v1261.zip Error downloading files: (Target directory already exists). Multi year stm32cube bug is still not fixed. Updated previously documented workaround method for this particular firmware update. ARG!
This error message is false since the zip file downloads but errors during extraction.
The folder inside stm32cube_fw_f4_v1261.zip is STM32Cube_FW_F4_V1.26.0 which I had already manually installed.
So I guessed and changed the subfolder name for v1261 from STM32Cube_FW_F4_V1.26.0 to
STM32Cube_FW_F4_V1.26.1.
My STM32Cube_FW_F4_V1.26.1 folder is only 17.6MB where the previous release of STM32Cube_FW_F4_V1.26.0 is 1.68 GB. So it seems like both packages need to be combined and only keep the newer 1.26.1 files? So I copied the files from the previous 1.26.0 release into the STM32Cube_FW_F4_V1.26.1 folder then overwrote any files found in the 1.26.1 release folder to see if that helped.
And it did. Now Stm32cubeIde appears happy and reported 1.26.1 was installed.
Please for the love of god fix this!! Thanks.