Skip to main content
Senior
Oct 16, 2025 4:50 PM UTC
Solved

Can't Run or Debug from CubeIDE

Hi

I don't know what happens, I just restarted my laptop, then it does not run or debug from CubeIDE. Before I retarted the laptop, I was debugging.When I click to Run or Debug, there is nothing appearing in the console window.  I closed the IDE twice, but nothing changed.

Anybody knows how to resolve this issue?

Chao

 

This topic has been closed for replies.
ChaoBest answer
Senior
Oct 17, 2025 7:12 AM UTC

The issue has been resolved by updating to 1.19.0 release of the CubeIDE.

Thanks to @AScha.3 , @TDK , and @Andrew Neil , especially @AScha.3 who has spent quite a lot time on this post.

Your help are highly apprecitaed!

Chao

21 replies

AScha.3
Super User
Oct 16, 2025 5:02 PM UTC

Hi,

wait, i just searching my large blue glass ball , then i can tell you what to do.

or

- which cpu / board you talk about ?

- what you did in detail ?

- show pic, connect with CubeProgrammer, what its telling.

- on which system ? 

- whats your last program ? used pins...needed debug pins ?

- any error messages ? 

 

If you feel a post has answered your question, please click on " Best Answer ".
ChaoAuthor
Senior
Oct 16, 2025 5:39 PM UTC

Thanks for the quick reply! 

I think it's nothing to do with MCU or board. I just launched the Cube Programmer and it can connect to the target F767 MCU on a customized board, programming is also OK. It can build my project.

I cleared the console, and then clicked on Debug button or Run button as shown in the following picture, nothing happens:

Chao_0-1760635534157.png

I have not seen any error message so far.

I have worked with CubeIDE for years, and this is the first time I come across this issue.

My laptop has 16GB memory running 64bit-windows 11 or 12.

 

 

AScha.3
Super User
Oct 16, 2025 6:20 PM UTC

Again...

>show pic, connect with CubeProgrammer, what its telling.

or 

if nothing responds in IDE...try delete its logs:

delete > .metadata/.plugins/org.eclipse.e4.workbench/workbench.xmi < , then it might (!) start again.

If you feel a post has answered your question, please click on " Best Answer ".
Andrew Neil
Super User
Oct 16, 2025 5:34 PM UTC

Where, exactly, do you click?

On this icon:

AndrewNeil_0-1760636009665.png

press the little down-arrow - is/are you debug config(s) listed?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ChaoAuthor
Senior
Oct 16, 2025 5:49 PM UTC

I alway click on the bug icon which will launch the debugger for the project listed on top, also for run icon. I also tried to click on the arrow and select the project on the top, but nothing happens in the console window.

I can also see a message of "Launching Tunnel: 0% with a progress bar flashing away quickly, this means I did click the bug icon successfully.

TDK
Oct 16, 2025 6:07 PM UTC

Try building the project. Does it build?

Reboot machine.

"If you feel a post has answered your question, please click ""Accept as Solution""."
ChaoAuthor
Senior
Oct 16, 2025 6:50 PM UTC

>Try building the project. Does it build?

It builds OK

>Reboot machine.

Tried twice already.

I clicked on most of the following icons, they all work except for the Debug and Run:

Chao_0-1760639932414.png

Before I restarted the machine, I was working with the debugger, I found my Serial Port Assistant software didn't work properly (it didn't print debugging text messages from my F767 board any more), so I decided to reboot the machine to resolve the issue (this usually works before), so I did the reboot, but when I launched the CubeIDE I found I can't run or debug from the IDE any more.