Skip to main content
Senior
July 21, 2024
Solved

Can't override a '__weak' function

Hi,

I write my own 'void HAL_SPI_TxRxCpltCallback(SPI_HandleTypeDef *hspi)', intend to override the default weak one. But when debug, my version is never called, it always steps into the 'weak' one. I'm new to CubeIDE, the version is 1.16.0, any suggestions?

Thanks.

    This topic has been closed for replies.
    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    July 21, 2024

    Using .cpp ?

    Double check spelling/capitalization

    Perhaps use objdump to inspect generated object from your source file.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

    4 replies

    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    July 21, 2024

    Using .cpp ?

    Double check spelling/capitalization

    Perhaps use objdump to inspect generated object from your source file.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    divergerAuthor
    Senior
    July 21, 2024

    Hi,

    My project is created as C++ project indeed. But my 'strong' version is defined in a ".c" file. Even I convert the project to 'C' project, my strong version won't be called. And I'm sure they have same signatures.

    BTW: does CubeIDE support 'objdump'? I'm on Windows system, not Linux.

    Tesla DeLorean
    Guru
    July 21, 2024

    I'm running GNU/GCC on Windows and have objdump and objcopy, and on Keil I have fromelf

    Y:\STM32\GNU>objdump
    Usage: objdump <option(s)> <file(s)>
     Display information from object <file(s)>.
     At least one of the following switches must be given:
     -a, --archive-headers Display archive header information
     -f, --file-headers Display the contents of the overall file header
     -p, --private-headers Display object format specific file header contents
     -P, --private=OPT,OPT... Display object format specific contents
     -h, --[section-]headers Display the contents of the section headers
     -x, --all-headers Display the contents of all headers
     -d, --disassemble Display assembler contents of executable sections
     -D, --disassemble-all Display assembler contents of all sections
     -S, --source Intermix source code with disassembly
     -s, --full-contents Display the full contents of all sections requested
     -g, --debugging Display debug information in object file
     -e, --debugging-tags Display debug information using ctags style
     -G, --stabs Display (in raw form) any STABS info in the file
     -W[lLiaprmfFsoRt] or
     --dwarf[=rawline,=decodedline,=info,=abbrev,=pubnames,=aranges,=macro,=frames,
    
     =frames-interp,=str,=loc,=Ranges,=pubtypes,
     =gdb_index,=trace_info,=trace_abbrev,=trace_aranges,
     =addr,=cu_index]
     Display DWARF info in the file
     -t, --syms Display the contents of the symbol table(s)
     -T, --dynamic-syms Display the contents of the dynamic symbol table
     -r, --reloc Display the relocation entries in the file
     -R, --dynamic-reloc Display the dynamic relocation entries in the file
     @<file> Read options from <file>
     -v, --version Display this program's version number
     -i, --info List object formats and architectures supported
     -H, --help Display this information
    
    Y:\STM32\GNU>objdump -v
    GNU objdump (GNU Tools for ARM Embedded Processors) 2.24.0.20141128
    Copyright 2013 Free Software Foundation, Inc.
    This program is free software; you may redistribute it under the terms of
    the GNU General Public License version 3 or (at your option) any later version.
    This program has absolutely no warranty.

    Not sure what CubeIDE brings in, but I'm not limited by that

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    TDK
    July 21, 2024

    Temporarily rename the weak one to something else, see if it compiles and links. Could be a misspelling in your strong version, or the string version isn't being compiled.

    "If you feel a post has answered your question, please click ""Accept as Solution""."