Skip to main content
Raees
Associate II
April 28, 2023
Question

Can't install STM32CubeIDE in Ubuntu 23

Getting the below error while installing

The following packages have unmet dependencies:

 st-stm32cubeide-1.12.1 : Depends: libpython2.7 but it is not installable

E: Unable to correct problems, you have held broken packages.

This topic has been closed for replies.

10 replies

Raees
RaeesAuthor
Associate II
April 28, 2023

I have manually installed libpython2.7 from the source code since it's not available in any package managers. You can see it's available in my machine from below terminal output. But this didn't solve the issue

ls /usr/local/lib/libpython2.7*

/usr/local/lib/libpython2.7.a  

/usr/local/lib/libpython2.7.so.1.0

/usr/local/lib/libpython2.7.so

Pavel A.
June 27, 2023

Yes it is invisible to apt exactly because it was installed manually. They should not have removed python2.7 packages. Or well... time to move to python3?

Visitor II
June 25, 2023

"I have the same problem, but with Kubuntu 23.04. Maybe someone from the ST company can help?"

Semer CHERNI
ST Employee
June 26, 2023

Hello @Raees 

First let me thank you for posting.

I am sorry to inform you that until this moment the the Ubuntu 23.04 is note yet supported.

The entire list of OS supported could be found in the release note RN0114.

KR,

Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Visitor II
October 17, 2023

I had the same problem, missing libraries/packages.
But after a bit of debugging, this sequence of steps solved it.

My system is:
Distributor ID: Debian
Description: Debian GNU/Linux 12 (bookworm)
Release: 12
Codename: bookworm

Steps:

wget http://ftp.de.debian.org/debian/pool/main/libf/libffi/libffi7_3.3-6_amd64.deb
wget http://security.ubuntu.com/ubuntu/pool/main/o/openssl/libssl1.1_1.1.1f-1ubuntu2.19_amd64.deb
wget http://ftp.de.debian.org/debian/pool/main/p/python2.7/libpython2.7-minimal_2.7.18-8+deb11u1_amd64.deb
wget http://ftp.de.debian.org/debian/pool/main/p/python2.7/libpython2.7-dev_2.7.18-8+deb11u1_amd64.deb
wget http://ftp.de.debian.org/debian/pool/main/p/python2.7/libpython2.7-dbg_2.7.18-8+deb11u1_amd64.deb
wget http://ftp.de.debian.org/debian/pool/main/p/python2.7/libpython2.7-stdlib_2.7.18-8+deb11u1_amd64.deb
wget http://ftp.de.debian.org/debian/pool/main/p/python2.7/libpython2.7_2.7.18-8+deb11u1_amd64.deb

dpkg -i libffi7_3.3-6_amd64.deb
dpkg -i libssl1.1_1.1.1f-1ubuntu2.19_amd64.deb
dpkg -i libpython2.7-minimal_2.7.18-8+deb11u1_amd64.deb
dpkg -i libpython2.7-stdlib_2.7.18-8+deb11u1_amd64.deb
dpkg -i libpython2.7-dbg_2.7.18-8+deb11u1_amd64.deb
dpkg -i libpython2.7_2.7.18-8+deb11u1_amd64.deb
dpkg -i libpython2.7-dev_2.7.18-8+deb11u1_amd64.deb


I don't recommend messing around with update-alternatives, it can seriously screw up your graphics environment.

Visitor II
October 27, 2023

hi ! your solution is quite useful. I use kubuntu/debian with 6.5 linux kernel.

if someone cannot install the libssl1.1_1.1.1f-1ubuntu2.19_amd64.deb. try to install this one.

http://security.ubuntu.com/ubuntu/pool/main/o/openssl/libssl1.1_1.1.1-1ubuntu2.1~18.04.23_amd64.deb

Explorer
October 18, 2023

I had the same problem on Ubuntu 23.04 with installations of versions 1.13.0, 1.13.01 and 1.13.2.
Version: you need to install not “STM32CubeIDE Debian Linux Installer”, but “STM32CubeIDE Generic Linux Installer”. Everything is going well!

Graduate II
July 10, 2024

Дякую!!!