Skip to main content
Associate III
Jul 23, 2024 9:47 PM UTC
Solved

Can't find Nucleo-MB1549 in board selection

I'm used to using the stm32cube-ide. I found a Nucleo-MB1549 in my attic and wanted to play around with it but i can't seem to find it in the board selector section. 

 

Any ideas what i should do next? This is a genuine nucleo board and i am able to find my other nucelo board using the application 

 

BadEngineer_0-1721771231250.png

 

    This topic has been closed for replies.
    TDK
    TDKBest answer
    Jul 23, 2024 11:29 PM UTC

    MB1549 is the board name, but the part number is either NUCLEO-U575ZI-Q or NUCLEO-U5A5ZJ-Q. Use the one that you have.

    TDK_0-1721777357078.png

    Should be a label on the board showing which one it is.

    "If you feel a post has answered your question, please click ""Accept as Solution""."

    2 replies

    TDK
    TDKBest answer
    Jul 23, 2024 11:29 PM UTC

    MB1549 is the board name, but the part number is either NUCLEO-U575ZI-Q or NUCLEO-U5A5ZJ-Q. Use the one that you have.

    TDK_0-1721777357078.png

    Should be a label on the board showing which one it is.

    "If you feel a post has answered your question, please click ""Accept as Solution""."
    Associate III
    Jul 24, 2024 5:35 AM UTC

    Thank you @TDK for your answer. I just got a bit confused because on the last STM32 project it said Nucelo on it and i was able to find the board quite easily