Skip to main content
hpipon957
Associate III
July 22, 2020
Question

Can't debug NUCLEO-F746ZG in STM32CubeIDE

Hi All

I can drag and drop a binary file to the NUCLEO-F746ZG via its mbed hard drive that appears when the board is connected to the PC and the program runs.

I can also try to debug from STM32CubeIDE and it successfully programs and verifies the code but it then always immediately loses connection with the following message:

...

Download verified successfully

(Read)Failed determine breakpoint type

Error! Failed to read target status

Debugger connection lost.

Shutting down...

The complete console output is below.

What could be causing this and how can it be solved????

Note that with IAR Kickstart the debugger works correctly so it must be an STM32CubeIDE setting problem(?)

Thanks

Regards

Mark

STMicroelectronics ST-LINK GDB server. Version 5.4.0

Copyright (c) 2019, STMicroelectronics. All rights reserved.

Starting server with the following options:

       Persistent Mode           : Disabled

       Logging Level             : 1

       Listen Port Number        : 61234

       Status Refresh Delay      : 15s

       Verbose Mode              : Disabled

       SWD Debug                 : Enabled

       InitWhile                 : Enabled

Waiting for debugger connection...

Debugger connected

     -------------------------------------------------------------------

                      STM32CubeProgrammer v2.3.0                 

     -------------------------------------------------------------------

ST-LINK SN : 066DFF545152717267241613

ST-LINK FW : V2J35M26

Voltage    : 3.24V

SWD freq   : 4000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID  : 0x449

Device name : STM32F74x/STM32F75x

Flash size : 1 MBytes

Device type : MCU

Device CPU : Cortex-M7

Memory Programming ...

Opening and parsing file: ST-LINK_GDB_server_a07064.srec

 File         : ST-LINK_GDB_server_a07064.srec

 Size         : 7746 Bytes

 Address      : 0x08000000

Erasing memory corresponding to segment 0:

Erasing internal memory sector 0

Erasing memory corresponding to segment 1:

Erasing internal memory sector 3

Download in Progress:

File download complete

Time elapsed during download operation: 00:00:01.402

Verifying ...

Download verified successfully

(Read)Failed determine breakpoint type

Error! Failed to read target status

Debugger connection lost.

Shutting down...

This topic has been closed for replies.

9 replies

Peter BENSCH
ST Technical Moderator
July 23, 2020

Did you initialize the debug pins?

If you didn't, then a download using SWD is possible, because after reset the pins are configured for SWD. But after that these pins are reinitialized as GPIO or whatever you set them to, so the connection gets lost.

Debugging requires these pins, so enable SYS > Debug > Serial Wire in CubeMX, if you want to debug.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
hpipon957
hpipon957Author
Associate III
July 23, 2020

Hi Peter

The program only sets the LED output and the user button input and otherwise leaves all pins in their default state. With IAR I can attach to the running target and debug so I don't think that it is a problem with SWD pins.

Today I managed a slight improvement with STM32CubeIDE in that after I have loaded the program (and the debugger disconnects) I then change the debugger configuration in the debugger configuration -> Startup -> Load Image and Symbols to "not perform the download" but still load symbols. Now I can connect to the board (which already has been programmed with the code) and I can run/pause and step code. However I can only step in "disassemble" mode since it says that it can't locate the source code (suggesting that it doesn't in fact correctly load the symbols).

Unfortunately it is also very unreliable in that sometimes it works and sometimes it just shows that it is running but it isn't and so I need to disconnect to start again.

Another thing to note is that after I load the program (attempting to debug) and it disconnects I tend to need to unplug the USB connector to get the board to respond again.

Finally if the loaded program is using the WFI command (to sleep between SYSTICKs) also the non-loading method doesn't connect/debug. This is however also an issue with IAR so I am presently avoiding using the WFI command when debugging.

I am using the most up to date STM32CubeIDE (installed a few days ago).

Do you have any ideas of other potential ways to try using it?

Regards

Mark

Peter BENSCH
ST Technical Moderator
July 23, 2020

If you are only debugging with the NUCLEO, it is strongly recommended to set the SWD pins.

There is also a debug setting "Connect under Reset" (usually default, check it with Run > Debug Configurations --> Tab: Debugger), which should also work, as after reset the pins PA13/PA14 (for STM32F746ZG) are set to SWD. See e.g. RM0385, section 6.3.1., currently at page 202.

Anyway, you can upload your IOC and maybe main.c + stm32f7xx_it.c, it shouldn't contain too much company secrets if you just control an LED and a button. We can then double-check what could be the reason. You could also upload the whole project as ZIP, but in that case please delete the folder Debug before, as it can be easily recreated.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
hpipon957
hpipon957Author
Associate III
July 23, 2020

Hi Peter

I was already using the "Connect under Reset" and I have also added PA13/PA14 configuration code immediately at startup but it doesn't change behavior.

With IAR I still have no issues and I can also debug the code (in disassembly mode) that STM32CubeIDE has programmed without any difficulties.

If you are interested in getting to the bottom of this the project is open source at https://github.com/uTasker/uTasker-Kinetis (don't be confused by the name since it allows NXP Kinetis projects to be moved to STM32 chips without porting effort).

To build with STM32CubeIDE:

  1. Clone the repository
  2. Copy the content of \Applications\uTaskerV1.4\STM32CubeIDE\Project_Settings to the root (that is where the folders like "Application", "Hardware", "stack" are located).
  3. Import the existing project from this location (don't import projects from sub-directories - i.e. just the one project)
  4. It is all set up for this target to build a simple "Blinky". If you want more functionality comment out the define BLINKY in \Applications\uTaskerV1.4\config.h and select things like file systems, the TCP/IP stack or USB, etc. Setting the define HELLO_WORLD will add USART output at 115k on the VCOM interface (to the simple blinky configuration).
  5. All is set up for the board so you you can just build without needing to configure anything.
  6. I didn't add a debug configuration since this is where it fails so maybe if you set one up it may behave differently but otherwise I expect it to do the same as I have reported. The green LED blinks at 2.5Hz.

Thanks

Regards

Mark

Peter BENSCH
ST Technical Moderator
July 24, 2020

Hi, Mark,

indeed a very interesting project.

Unfortunately I don't find the time to dig into the issue, maybe someone else is able to jump in.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
hpipon957
hpipon957Author
Associate III
July 24, 2020

Hi Peter

It is a shame that you won't have time to check out the problem but we will wait to see whether someone with more experience than us can take a look.

In the meantime we have reverted back to Atollic TrueSTUDIO (which was previously offered by ST-Micro) which works without any issues [also when using sleep modes between interrupts with WFI instruction] (project also in the open source project) and will try again later when new versions of STM32CudeIDE have been released which may have fixed something.

I did spend some more time with STM32CubeIDE this morning to see whether I could find a workaround and can (when downloading is disabled) do limited debugging (also in source code after changing the debug level) but the debugger loses the connection very easily, leaving the board running and needing to reconnect again (and start again). Therefore the experiences seem to confirm that something is too unstable at the moment.

Regards

Mark

ozcan
Visitor II
July 28, 2020

I have been working on some projects using STM32CubeIDE v1.3.0 version for a long time (OS: macOS Catalina). Unfortunately, I updated STM32CubeIDE to v1.4.0 this morning and IDE couldn't find ST-link Server. Even after I manually tried to update ST-LINK server software module 1.3.0, it didn't work... (It can be about Catalina's /Application folder permissions but I am not sure.)

Long story short, I have just switched back to v1.3.0 (no issues about debug or connecting to ST-link Server) after wasting about 5 hours.

hpipon957
hpipon957Author
Associate III
July 28, 2020

Hi

Although I installed only a few days ago I see that I have 1.2.0 (for Windows). Maybe the MAC version(s) have different version numbers?

Regards

Mark

Peter BENSCH
ST Technical Moderator
July 28, 2020

Please check the website for STM32CubeIDE, where you find the current version. Some previous ones are also available when selecting the required version using the dropdown button on the right.

Good luck

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.