Skip to main content
This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
February 20, 2022

Does the F413 even have support for Ethernet? Where would that connection come from? Cellular Modem, WiFi?

You can likely find a TCP/IP stack with support of assorted protocols. Commercial offerings likely to have a richer set of examples and support.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
STAHI.1
STAHI.1Author
Associate
February 21, 2022

in my project i use stm32F413ZHT6+w5500

mattias norlander
ST Technical Moderator
February 25, 2022

Not something that is officially supported in the Cube ecosystem.

w5500 seem to have SPI interface...

I think this setup will imply a lot of work without much support.

But if you are lucky maybe you can google and find some examples that already work well.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.