Skip to main content
Jens1
Visitor II
Dec 15, 2019 6:59 PM UTC
Question

C++ Support in STM32CubeIde - class symbol not accepted

Hello All,

I made a C/C++ project with STM32CubeIde version 1.1.0. It works fine.

Then I added a C++ class by a cpp and hpp file. And tried to make an instance of the class in the main.c file. The compiler does not recognize "class" symbol in my hpp file. How to solve this?

Is there an coding example?

Thanks and regards,

Jens

arm-none-eabi-gcc "../Core/Src/main.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DUSE_HAL_DRIVER -DDEBUG -DSTM32F429xx -c -I../Middlewares/Third_Party/FreeRTOS/Source/include -I../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM4F -I../Drivers/CMSIS/Include -I../Drivers/STM32F4xx_HAL_Driver/Inc -I../Core/Inc -I../Drivers/CMSIS/Device/ST/STM32F4xx/Include -I../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS -I../Drivers/STM32F4xx_HAL_Driver/Inc/Legacy -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Core/Src/main.d" -MT"Core/Src/main.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Core/Src/main.o"

In file included from ../Core/Src/main.c:25:0:

../Core/Src/CFlashLed.hpp:21:1: error: unknown type name 'class'

 class CFlashLed

 ^~~~~

../Core/Src/CFlashLed.hpp:22:1: error: expected '=', ',', ';', 'asm' or '__attribute__' before '{' token

This topic has been closed for replies.

3 replies

KnarfB
Super User
Dec 15, 2019 9:35 PM UTC

A .c file is considered to contain C source code, not C++ and class is not a keyword in C. What you can do, is calling a C++ free function in a separate .cpp file from main() which in turn instantiates an object of you class.

ywang.1
Visitor II
May 8, 2021 2:19 AM UTC

rename main.c to main.cpp​