Skip to main content
RAltm
Senior
September 25, 2020
Question

C++: how are 'new' and 'delete' operators implemented by default?

Hello,

I'm porting a C++ application to a STM32 device. The application itself is running, but I'm observing heap memory growing into the stack and firing an exception after a while. Running the application on Windows within Visual Studio shows the same behaviour regarding used memory going only up, but without crashing. This might be because there are GB of RAM instead of kB ;)

But I doubt that the application has memory leaks, I think that Windows is kidding me. The application is originally written on a Mac device. I'm in contact with the author and he couldn't see this behaviour on his setup and also never had crashes.

So, I assume I'm missing some compiler settings or something like that and I want to investigate the issue. I saw some articles regarding C++ on embedded devices and they recommend to overwrite the new and delete operator to use malloc() and free(). If I'd do this, I would also output a message how many memory is requested and freed. But I want to know the default implementation of the new and delete operators to check how they work. Where can I find those informations?

Thank you.

Regards

This topic has been closed for replies.

14 replies

Pavel A.
September 25, 2020

The default operator new is basically a wrapper around malloc and uses the same heap.

If this app needs amount or RAM not available on STM32, or leaks memory - game is over.

Does that guy test his app on a similar ARM 32-bit? Yes, WIndows or OSX has GBs of RAM and it matters.

If you use threads (some RTOS) - the runtime library provided with CubeIDE does not support threads. You'll need to find a workaround.

-- pa

Nikita91
Lead II
September 25, 2020

As far as I know, new / delete uses newlib's native _malloc_r() / _free_r() functions. Who themselves use the _sbrk() (or _sbrk_r()) function in syscalls.c

The redefinition of the _malloc_r() / _free_r() functions by the user allows you to manage the memory allocation yourself (the presence of your functions prevents the linker to link the newlib functions).

if your _malloc_r() / _free_r() are not thread safe, you have to implement __malloc_lock()  and __malloc_unlock()

https://tty.uchuujin.de/2016/04/stm32-from-scratch-heap/

https://stackoverflow.com/questions/19258847/stm32-c-operator-new-coide

Some infos about malloc and newlib:

http://www.nadler.com/embedded/newlibAndFreeRTOS.html

RAltm
RAltmAuthor
Senior
September 25, 2020

@Pavel A.​ 

No, he can't test it on ARM devices. There was never an embedded bare-metal target in scope when whe wrote this application. And the application doesn't use threads.

@Nikita91​ 

Thank you for those links, I'll go through them. If new and delete really use malloc() and free() and nothing else, I think overwriting them with additional output capabilities shouldn't be a problem. I wrote a _sbrk() implementation at the beginning of the project, as well as some other functions needed by library/project. I assume(!) this _sbrk() implementation is working correctly. At least it looks okay for me, but I'm a beginner with newlib internals.

So, both C and C++ use newlib in general, is this true?

Regards

Nikita91
Lead II
September 25, 2020

You can instrument _sbrk() to track the count and size of malloc. Not with printf, but with SWO or direct output to an UART.

Programming Windows or microcontrollers are not the same job...

RAltm
RAltmAuthor
Senior
September 25, 2020

Yes, should be no problem with SWO. I know that this is not the same :) I've more experience with programming MCUs. Sometimes, when I see source code for desktop OS I think 'what a waste of memory'. I learned MCU programming on 8052s with assembler, so memory was always rare...

RAltm
RAltmAuthor
Senior
September 26, 2020

Hmm... seems the SWO output is disturbed. Not much, but some packets are lost. Maybe using a delay will help.

Back to the original question, is there any source which shows how the default operations are implemented?

Regards

Nikita91
Lead II
September 26, 2020

You have to dig in newlib source code.

The newlib vesion distributed with CubeIDE is 3.0.0:

ftp://sourceware.org/pub/newlib/newlib-3.0.0.tar.gz  (81ec873108b8593c586f91ca65963952)

The newlib vesion distributed with Atollic 9.3.0 is 2.5.0

ftp://sourceware.org/pub/newlib/newlib-2.5.0.tar.gz

RAltm
RAltmAuthor
Senior
September 28, 2020

Hi Nikita,

thank you for those links, I'll go through them and try to figure out how the memory management is working. Currently it seems that the heap is only growing upward, but never goes down. This measurement was taken within _sbrk() function, output was written into a character array by snprintf() - for this function I assume(!) that it won't use dynamic memory. Even if this is not true, I'd assume that I should see a negative increment within _sbrk() at least sometimes.

Regards

Nikita91
Lead II
September 29, 2020

There is never negative increment to _sbrk.

Once a block is taken from _sbrk, it is managed by malloc.

Functions of the printf family use malloc ... So beware of recursivity.

Uwe Bonnes
Chief
September 29, 2020

For an embedded device, carefully consider the use of dynamically allocated memory. During setup, you can do it. But using it during runtime probably will hit a memory limit at some point in time and that will be hard to debug.

RAltm
RAltmAuthor
Senior
September 29, 2020

@Nikita91​ 

Documentation about _sbrk() states that it's possible that _sbrk() gets a negative value passed to it. So, your statement applies to newlib? I mean, in newlib it won't get a negative value?

You're right, I did not think of recursivity. For the printf function, I think I'll write a small one for the output I need. Since I only want to output decimal values, I think it should be possible without using dynamic memory.

@Uwe Bonnes​ 

Since I want to port an existing C++ application, I've no choice :) And I'm hitting the limit. Now I'm trying to figure out why. I agree that dynamic memory should be used carefully, but this is also the case on a non-embedded system.

Regards

Nikita91
Lead II
October 4, 2020

Where do you see the increment can be negative ?

Did you check the _sbrk implementation in sycalls.c to know if negative increment is properly managed ?

Pavel A.
October 4, 2020

> For the printf function, I think I'll write a small one for the output I need.

Why printf?! You're using c++.

-- pa