Skip to main content
JGurley
Associate
Jul 31, 2025 8:19 PM UTC
Question

Build GNU Tools for STM32 12.3.rel1

Hello :)

I am wondering if there is a "how to" for how to build the stdlibc++ library for STM32 gcc tools.  I am in need of a stripped down stdlibc++ library to link with.  Can anyone point me to a link or can you walk me through it?

The reason I ask, is because my compiled binary has included things like std::__cxx11::time_get and std::time_get.  There are 8 instances of this variant each with 2.76K in size.  We are using c++ but we certainly aren't using anything related to time.  Locale is another thing we aren't using.  There are two instances of std::locale::_Impl::_Impl(unsigned it) which is 1.82K in  size as well.  

These functions appear in the binary even though we are using compiler flags -ffunction-sections -fdata-sections and linker flags -Wl,--gc-sections.

I need to get rid of the "fluff" that isn't used from libstdc++. I would like to build libstdc++ with -ffunction-sections -fdata-sections flags so the linker can remove the unused sections when it links libstdc++.  And perhaps build without locale and time since those are both build flags and are parts of the library that we don't and won't need.

This topic has been closed for replies.

1 reply

Pavel A.
Aug 1, 2025 6:07 PM UTC

Have you seen this with previous toolchain versions?