Skip to main content
Associate
Dec 20, 2024 3:22 PM UTC
Question

Build GNU Tools for STM32 12.3.rel1

I am trying to build the toolchain and I'm looking for some help getting over this hurdle.

When I run build-prerequisites.sh on Ubuntu, it stops when it tries to run "helper.py" with the error "You need to install python-magic."  Helper.py is running python3 which I've tried linking to Python3.4, 3.5, 3.8, etc.  If I change it to use Python2, it gets over this error but fails with a different one regarding a FILE==STDERR parameter being passed to the Print function (I'm not a Python guy).

Just starting Python2 and typing the line "Import Magic" works.  Any other Python does not work.

Let me also put out that what I am really trying to do is get the sources for all the running code so when I debug I can debug into the function.  It might be that I can just take that "src" directory and park it somewhere and get the same result, but it's more figuring out than I have time for.

I only need the build for Windows also and I assume I need the "debug" type but there is zero documentation.

The version I downloaded from GitHub is this:

Release GNU Tools for STM32 12.3.rel1.20240926-1715

Thanks in advance for your help.

donkharrison

This topic has been closed for replies.

2 replies

Pavel A.
Dec 20, 2024 4:34 PM UTC

> it stops when it tries to run "helper.py" with the error "You need to install python-magic."

It is available here: https://pypi.org/project/python-magic/

> what I am really trying to do is get the sources for all the running code so when I debug I can debug into the function.

So you need to build only the newlib. Even do not build it, maybe just looking at the sources can be enough.

 

Associate
Dec 20, 2024 5:40 PM UTC

I have installed python-magic, but when I am running python3, it will not execute "Import magic."

I'm not sure what newlib is other than what Wikipedia told me, or how I would use it.  I can see that it is part of the build, and I can see that I can make it independent of the build (seemingly).

In the end, I need the STM32CubeIDE to have access to the sources when I single step outside the scope of my code.