Skip to main content
Visitor II
Jun 24, 2025 3:39 AM UTC
Question

Build error - STSW-KITSTKNX

Hi, Sir/Marm,

I tried to build STSW-KITSTKNX according to the instruction described in the document UM2409.

But it failed.

Could you please give me a solution for it?

[ Project ] EvalKitSTKNX_inOut4

 - Error detail : After clean project  

make: *** No rule to make target 'clean'. Stop.

 

12:17:27 Build Failed. 1 errors, 0 warnings. (took 477ms)

 

- Error and worning detail : After build project

C:/STeval_STKNX/en.STSW-KITSTKNX/STSW-KITSTKNX/Libraries/Tapko/dev_mod/07B0/dat_07B0.c:87:1: warning: ignoring attribute 'section ("BCU_EEPROM")' because it conflicts with previous 'section ("BCU_SYS_EEPROM")' [-Wattributes]

C:/STeval_STKNX/en.STSW-KITSTKNX/STSW-KITSTKNX/Project/STM32F10x_STKNX_inOut4/Src/app_data.c:70:1: warning: ignoring attribute 'section ("BCU_EEPROM")' because it conflicts with previous 'section ("BCU_SYS_EEPROM")' [-Wattributes]

(.text._close_r+0xc): warning: _close is not implemented and will always fail

C:/ST/STM32CubeIDE_1.18.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.18.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/lib/thumb/v7-m/nofp\libc_nano.a(libc_a-closer.o): note: the message above does not take linker garbage collection into account

C:/ST/STM32CubeIDE_1.18.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.18.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/lib/thumb/v7-m/nofp\libc_nano.a(libc_a-fstatr.o): note: the message above does not take linker garbage collection into account

(.text._fstat_r+0xe): warning: _fstat is not implemented and will always fail

(.text._getpid_r+0x0): warning: _getpid is not implemented and will always fail

(.text._isatty_r+0xc): warning: _isatty is not implemented and will always fail

C:/ST/STM32CubeIDE_1.18.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.18.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/lib/thumb/v7-m/nofp\libc_nano.a(libc_a-signalr.o): note: the message above does not take linker garbage collection into account

C:/ST/STM32CubeIDE_1.18.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.18.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/lib/thumb/v7-m/nofp\libc_nano.a(libc_a-isattyr.o): note: the message above does not take linker garbage collection into account

(.text._kill_r+0xe): warning: _kill is not implemented and will always fail

C:/ST/STM32CubeIDE_1.18.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.18.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/lib/thumb/v7-m/nofp\libc_nano.a(libc_a-signalr.o): note: the message above does not take linker garbage collection into account

(.text._lseek_r+0x10): warning: _lseek is not implemented and will always fail

C:/ST/STM32CubeIDE_1.18.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.18.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/lib/thumb/v7-m/nofp\libc_nano.a(libc_a-lseekr.o): note: the message above does not take linker garbage collection into account

(.text._read_r+0x10): warning: _read is not implemented and will always fail

C:/ST/STM32CubeIDE_1.18.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.18.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/lib/thumb/v7-m/nofp\libc_nano.a(libc_a-readr.o): note: the message above does not take linker garbage collection into account

(.text._write_r+0x10): warning: _write is not implemented and will always fail

C:/ST/STM32CubeIDE_1.18.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: warning: EvalKitSTKNX_inOut4.elf has a LOAD segment with RWX permissions

C:/ST/STM32CubeIDE_1.18.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.18.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/lib/thumb/v7-m/nofp\libc_nano.a(libc_a-writer.o): note: the message above does not take linker garbage collection into account

 

12:17:50 Build Failed. 8 errors, 11 warnings. (took 22s.54ms)

 

This topic has been closed for replies.

2 replies

Billy OWEN
ST Employee
Jun 24, 2025 8:11 PM UTC

Hi @Seiji 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy

Shubhendu Banerjee
Associate II
Jun 27, 2025 4:46 PM UTC

I'm also getting the same errors. Previously, I had to define _write only to print things. Now, with STM32CubeIDE Version 1.18.1, to compile the project successfully, I need to create a few stubs.
    Additionally, when I put the stubs in a .c, the .c gets deleted every time  I generate code with .ioc.

 

#include <errno.h>
#include <sys/types.h>
#include <sys/stat.h>
#include <unistd.h>

//
#include "usart.h"

int _write(int fd, char *ptr, int len) {
    HAL_UART_Transmit(&huart1, (uint8_t*) ptr, len, HAL_MAX_DELAY);
    return len;
}

// Stub for _read
ssize_t _read(int file, void *ptr, size_t len) {
    errno = EBADF;
    return -1;
}

// Stub for _close
int _close(int file) {
    return -1;
}

// Stub for _lseek
off_t _lseek(int file, off_t ptr, int dir) {
    return 0;
}

// Stub for _fstat
int _fstat(int file, struct stat *st) {
    st->st_mode = S_IFCHR;
    return 0;
}

// Stub
int _getpid(void) {
    return 1;  // or 0, any dummy PID
}

// Stub
int _kill(int pid, int sig) {
    errno = EINVAL;
    return -1;
}

// Stub for _isatty
int _isatty(int file) {
    return 1;
}