Associate II
June 7, 2019
Question
Bug with single wire UART
- 0 replies
- 765 views
Hey there,
it's no big deal, but rather annoying. If I select one UART to be Half-Duplex the RX pin disappears from the pinout even if I select receive only. It doen't matter if I select RX only or TX only, the RX-pin won't show up again. The generated code also initializes only the TX pin. Boooo.
I'm using STM32CubeIDE
Version: 1.0.0
Build: 2872_20190423-2022 (UTC)