Skip to main content
KNaim.1
Associate III
May 9, 2025 6:32 PM UTC
Solved

Bug STM32 cube ide stm32h743

 

Many try to restart computer clean the project rebuild that the second time that make me crasy!!!!!!

 

 

STMicroelectronics ST-LINK GDB server. Version 7.10.0

Copyright (c) 2025, STMicroelectronics. All rights reserved.

 

Starting server with the following options:

Persistent Mode : Disabled

LogFile Name : C:\Users\domoledlight\STM32CubeIDE\workspace_1.15.1\STM32h7432024\Debug\st-link_gdbserver_log.txt

Logging Level : 31

Listen Port Number : 61234

Status Refresh Delay : 15s

Verbose Mode : Enabled

SWD Debug : Enabled

 

COM frequency = 4000 kHz

Target connection mode: Attach

Reading ROM table for AP 0 @0xe00fefd0

Hardware watchpoint supported by the target

ST-LINK Firmware version : V2J45S7

Device ID: 0x450

PC: 0xfa0

ST-LINK device status: LOCKUP

Enter STM32_SystemReset() function

ST-LINK detects target voltage = 3.16 V

Device in lock up state, possibly "read and debug" protected. Use monitor commands to remove the protection

ST-LINK device initialization OK

Stm32Device, pollAndNotify running...

ST-LINK device status: HALT_MODE

SwvSrv state change: 0 -> 1

Waiting for debugger connection...

Waiting for connection on port 61234...

Waiting for connection on port 61235...

Accepted connection on port 61234...

Debugger connected

Waiting for debugger connection...

Waiting for connection on port 61234...

GDB session thread running

GdbSessionManager, session started: 1

Accepted connection on port 61234...

Debugger connected

Waiting for debugger connection...

Waiting for connection on port 61234...

GDB session thread running

GdbSessionManager, session started: 2

Accepted connection on port 61235...

SWV collect poll delay set to 3413µs for baudrate 2000000Hz (buffer size 2048b)

SwvSrv state change: 1 -> 2

GDB session terminated: Client connection lost

GdbSessionManager, session terminated: 1

GDB session terminated: Client connection lost

GdbSessionManager, session terminated: 2

GdbSrv, last session terminated, signal dispose

Stopping port 61234

Cleanup session: 1

Cleanup session: 2

GDB session disposed: 1

GDB session disposed: 2

SwvSrv state change: 2 -> 1

SwvSrv session thread disposed

Waiting for connection on port 61235...

Received stop for port 61234, not accepting new connections.

GdbSrv, deInit entry.

Shutting down...

GdbSessionManager, deInit entry.

GdbSessionManager, deInit exit

SwvSrv deInit entry

Stopping port 61235

Stopping port 61234

Received stop for port 61235, not accepting new connections.

SwvSrv deInit exit

Stm32Device, closeDevice() entry

Stm32Device, pollAndNotify stopped

Stm32Device, closeDevice() exit

Stm32Device, deInit success

GdbSrv, deInit exit.

Exit.

many try to restart computer clean the project rebuild that the second time that make me crasy!!!!!!

This topic has been closed for replies.
KNaim.1
KNaim.1Best answer
Associate III
May 21, 2025 8:57 AM UTC

i have rebuild a new project

2 replies

KDJEM.1
ST Technical Moderator
May 16, 2025 10:06 AM UTC

Hello @KNaim.1 ;

 

Could you please give more details about the issue? Which STM32CubeIDE are you using? Are you use a ST board or customer board?  Have you tried running an example for STM32CubeH7 firmware?

Please look at How to write your question to maximize your chances to find a solution.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
KNaim.1
KNaim.1AuthorBest answer
Associate III
May 21, 2025 8:57 AM UTC

i have rebuild a new project