Break at address "0x429a683a" with stm32f469zi
Hi I'm trying to program a custom board with an stm32f469zi. Whenever I try to enter HAL_Init() at the very beginning of the code, I keep getting this error while trying to go through debugging:
Break at address "0x429a683a" with no debug information available, or outside of program code.
I set some breakpoints and traced it back to HAL_MspInit() where it contains this line of code:
HAL_NVIC_SetPriority(PendSV_IRQn, 15, 0);
I followed that even further (because the rest of the code works fine, I was following the trail of breaks) to NVIC_EncodePriority () under core_cm4.h. This function has a parameter called SubPriority where SubPriorityBits gets added onto it. It's precisely the line where SubPriorityBits gets all its bits but I'm not sure what this all means.
Is my project collapsing when it is trying to set up one of the interrupts? I have three global interrupts enabled in cubeMX: LTDC, DMA2D, and DSI.