Basic link using F3?
I am coming at the cubeIDE as a newbie AND as a hardware guy. With that said can someone tell me why when I am on a function / header file / or even a #define that SOMETIMES when I hit the F3 on the keyboard I do not jump to the corresponding definition? I realize it's a simple question (am coming from a Code Composer Studio background and it always seems to jump to the link).....I am guessing it could be I don't have something set up correctly in cubeIDE?? For instance I downloaded the BLE_p2pServer project.....Within this I go to the SystemClock_Config function where they call the following...__HAL_RCC_LSEDRIVE_CONFIG. If I place my cursor there and hit F3 nothing happens BUT I have a similar project that I am working in with an identical call and when I hit F3 with cursor on function I jump right to the file...I downloaded and installed this from github....The intereseting thing is if I right click on properties of this project I don't have options for C/C++ Build.
Thanks
Steve