Skip to main content
DGrön.1
Associate
Feb 4, 2025 2:06 PM UTC
Question

Bad serial com on STM32H753IITx with later FW

Code which have worked well like a year ago with FW, MX and IDE versions that were current at that time does not work now.

The problem comes after a call to HAL_UART_Transmit with one byte ("C") to transmit. After it is transmitted and while the counterpart is transmitting a response packet, (Ymodem packet 0), the response packet is garbled by STM transmitting spurious "C" characters with intervals between 0.1 and 1.1 s.

I am using UART5 async mode, hardware flow control RS485, 57600 bps.

Current versions:

MX 6.13.0

FW 1.8.0, 1.11.1, 1.11.2, 1.12.1

IDE 1.17.0

 

This topic has been closed for replies.