Skip to main content
JLee.32
Associate III
July 23, 2021
Question

assertion "REENT malloc succeeded" failed

  • July 23, 2021
  • 6 replies
  • 3563 views

After upgrading CubeIDE from 1.3.0 to 1.6.1 and CubeMx from 5.6.1 to ​6.2.1. I got this error:

assertion "REENT malloc succeeded" failed: file "/build/gnu-tools-for-stm32_9-2020-q2-update.20201001-1621/src/newlib/newlib/libc/time/lcltime.c", line 50

MCU: STM32H750

How to reproduce: Send the BLE message from mobile to BLE chip(QN9021). The BLE chip is connected to MCU via UART.

Any advice would be appreciated.

This topic has been closed for replies.

6 replies

JLee.32
JLee.32Author
Associate III
July 31, 2021

@mattias norlander​ 

I found the issue is happend while using new toolchain(gnu-tools-for-stm32_9-2020-q2-update...). If i switch back to the other installed toolchain (2018), it works fine. I saw you solved some toolchain issues, so could you help to check this issue?

Amel NASRI
ST Technical Moderator
August 4, 2021

Hi @JLee.32​ ,

Latest STM32CubeIDE version is 1.7.0. Is initially reported issue still faced with this version?

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
JLee.32
JLee.32Author
Associate III
August 9, 2021

@Amel NASRI​ 

Yes, the issue is still faced with 1.7.0.

Amel NASRI
ST Technical Moderator
August 9, 2021

Hi @JLee.32​ ,

Thanks for your answer. In such case, I let our CubeIDE experts (@Markus GIRDLAND​ & @mattias norlander​ ) investigate the issue.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
JLee.32
JLee.32Author
Associate III
August 10, 2021

Hi @Markus GIRDLAND​  & @mattias norlander​ ,

I found the root cause is that localtime() is used in the task of freertos. localtime() calls malloc() which returns -1 due to _sbrk(). Using localtime_r() is one solution, but I'm wondering if we can overwrite the standard version of malloc? Please see this link. I add the following code at main.c and main.h, but it shows error. How should I do to overwrite the standard version of malloc?

https://www.freertos.org/FreeRTOS_Support_Forum_Archive/October_2009/freertos_malloc_function_in_FreeRTOS_3444349.html

~~~~~

/* Defining malloc/free should overwrite the standard versions provided by the compiler. /

void malloc (size_t size)

{

/* Call the FreeRTOS version of malloc. */

return pvPortMalloc( size );

}

void free (void* ptr)

{

/* Call the FreeRTOS version of free. */

vPortFree( ptr );

}

~~~~~

Regards,

Jimmy

Markus GIRDLAND
ST Employee
August 16, 2021

Hello Jimmy,

If you implement your own malloc it could be called before the application which might not be OK, depending on the application.

There were changes made to the _sbrk() (sysmem.c) in newer versions of STM32CubeIDE and the easiest way could be to generate a new project and copy over the updated version file with the _sbrk() function.

The application might also not be thread safe and you it's likely you would need to thread safe it, which you could do at the same time you update the _sbrk().

Also, it might be a bit unlikely, but it could be as simple as not using newlib nano. Even if that helps I would still recommend using an updated version of the _sbrk() function.