Skip to main content
KLoma
Visitor II
July 29, 2019
Question

As I understand installation package en.st-stm32cubeide_1.0.2_3566_20190716-0927_x86_64.exe is suitable for both 32-bit and 64-bit Windows. Thanks in advance! Konstantin

..

This topic has been closed for replies.

1 reply

Markus GIRDLAND
ST Employee
July 30, 2019

CubeIDE only works on 64-bit Windows as it is part of the x86_64 architecture. You should receive an error if you try to launch it on a 32-bit Windows.

We are looking into some solutions to make this more clear for the user such as mentioning it on the website or possibly renaming future installers, but the 64-bit only requirement will remain.