Skip to main content
Associate
July 3, 2024
Solved

As a result of updating CubeIDE to V1.16.0, program transfer to MCU inevitably fails.

After updating CubeIDE to V1.16.0, I get an error like "Data mismatch found at address 0x08001000 (byte = 0xFF instead of 0x0E)" and cannot complete the debugger. This error text was obtained from the Internet with similar symptoms, except for the address number, etc.
I have tried all the solutions available on the Internet, but none of them worked. I also installed and tried CubeIDE released in the past, but it did not work.
Before the update, I was able to complete the debugger reliably.

Development Environment
CubeIDE V1.15.1 or V1.16.0
ST Link V3MINIE

This topic has been closed for replies.
Rim LANDOLSI
Rim LANDOLSIBest answer
ST Employee
July 3, 2024

Hello @neginegi885  and welcome to the community,

 

Could you specify the MCU used and have you done an ST-Link upgrade?

Thanks,

Rim.

7 replies

Rim LANDOLSI
Rim LANDOLSIBest answer
ST Employee
July 3, 2024

Hello @neginegi885  and welcome to the community,

 

Could you specify the MCU used and have you done an ST-Link upgrade?

Thanks,

Rim.

Associate
July 4, 2024

But it didn't work.

Rim LANDOLSI
ST Employee
July 4, 2024

Could you try to flash the program with STM32Cube programmer standalone? And if it is possible to share the elf file of the project?

Associate
July 4, 2024

MCU: STM32F723VET6

The update of ST-Link is complete.

 

Apologies: I chose the best answer by mistake...
My apologies...