Absolute noob: how to determine the pin that the LED is on in the IDE?
I'm using a Nucleo -64 stm32f030r8 board.
I've looked at various "blinky" tutorials and they all seem to just pick a a pin out of the air as the LED pin and then flash it through HAL_Toggle_Pin. I have the datasheet for the device but I seem to be blind, stupid and/or a combination of the two.
Can some kind soul step me through the "process" you use to determine which pin ld2 (the green led) is on? I created an stm32 project from the IDE wizard selecting the correct board but no pin is assigned as default as the LED. I can compile, upload and debug etc, it's just me not being able to figure out the LED assignment. Something very obvious I'm sure!
(as a side note, the IDE runs really poorly on my Debian testing desktop and frequently crashes but I can cope with that for now).