Skip to main content
DVolp.5
Visitor II
July 31, 2019
Question

A simple question. How change the SWD frequency, in the Debug Configurations, with ST-LINK GDB Server?

There are Initialization commands that can to do this?

Maybe another way?!

Tks,

Diego Volpini

This topic has been closed for replies.

1 reply

Uwe Bonnes
Chief
August 1, 2019

> ./STM32_Programmer_CLI

Usage :

STM32_Programmer_CLI.exe [command_1] [Agruments_1][[command_2] [Agruments_2]...]

... -c,    --connect     : Establish connection to the device

    <port=<PortName>  : Interface identifer. ex COM1, /dev/ttyS0, usb1,

                         JTAG, SWD...)

   UART port optional parameters: 

    [br=<baudrate>]   : Baudrate. ex: 115200, 9600, etc, default 115200

    [P=<parity>]      : Parity bit, value in {NONE,ODD,EVEN}, default EVEN

    [db=<data_bits>]  : Data bit, value in {6, 7, 8} ..., default 8

    [sb=<stop_bits>]  : Stop bit, value in {1, 1.5, 2} ..., default 1

    [fc=<flowControl>] : Flow control

                         Value in {OFF,Hardware,Software} ..., default OFF

    [noinit=noinit_bit]: Set No Init bits, value in {0,1} ..., default 0

   JTAG/SWD debug port optional parameters: 

    [freq=<frequency>] : Frequency in KHz. Default frequencies:

                         4000 SWD 9000 JTAG with STLINKv2

                         24000 SWD 21333 with STLINKv3