Skip to main content
AKhot.1
Associate III
September 4, 2023
Solved

2D-FFT rfft and cfft functions

I have a 2D array input buffer. so, what is the correct way to implement the rfft and cfft functions?

float fftIn[16][512] is my input. So, I applied for a loop like below:

arm_rfft_fast_init_f32(&fftHandler, 512);

 

for(int d =0; d<16; d++){
arm_rfft_fast_f32(&fftHandler, &fftIn[d], &fftOut[d], 0);
}
Is this the correct way?
Since the fftout will be complex no. I have taken cfft along the column(by rearranging the 2d array in certain way) like below:
Here input is like fft2In[256][32]
for(int e = 0; e<256; e++){
arm_cfft_f32(&arm_cfft_sR_f32_len16, &fft2In[e], 0, 0);
}
Again is the correct way to implement? I am getting some output but I don't have a way to verify the result as of now.
Please help me with this?
 

 

This topic has been closed for replies.
AKhot.1
AKhot.1Best answer
Associate III
September 6, 2023

For those of you who might need help with 2D FFT, this is the correct approach.

3 replies

AKhot.1
AKhot.1Author
Associate III
September 5, 2023

Can anyone explain this?

Bob S
Super User
September 5, 2023

No help directly, but the first (or second) rule of algorithm development and testing is to have a known input data and the expected output, preferably multiple sets of inputs and outputs.  Without that you are just wasting your time.

AKhot.1
AKhot.1AuthorBest answer
Associate III
September 6, 2023

For those of you who might need help with 2D FFT, this is the correct approach.