Skip to main content
Visitor II
May 6, 2026 12:55 AM UTC
Question

VSCode Extension v3.9.0 Breaks Debugger

Device: NUCLEO-N657X0-Q Board
 
Environment: STM32CubeIDE for Visual Studio Code Extension (v3.9.0)
 
Description & Symptoms: The debugger loses a connection with the board with “Target not responding” and “Unable to read memory” errors.  Reverting to version v3.8.0 of the extension and all of its dependencies resolves the issue.
 
Steps to Reproduce:
  1. Set a breakpoint on the first line of the FSBL Reset_Handler
  2. Run the debugger
  3. Step past the following line in the Reset_Handler: mov sp, r0
 
Expected Behavior: Debugger is able to continue stepping through the code
 
Actual Behavior: The device stops responding and is unable to reconnect until unplugging and plugging back in
 
Other Notes: When running the debugger without a breakpoint set, the program runs normally.  As soon as a breakpoint is set, it loses the connection.

2 replies

Associate II
May 6, 2026 1:57 AM UTC

Coincidentally I just had this issue myself and somebody on another forum was able to guide me with the same solution.

I was able to narrow down the problematic extension to be the STM32 Debug Core by updating every other extension apart from that one while keeping debugging capabilities. I specifically tested this with the Nx_TCP_Echo_Server example with my STM32N6 Nucleo.

LaurentL
ST Employee
Jun 17, 2026 12:47 PM UTC

Hello,

See the post :

Your issue on STM32N6 has been fixed.

You can update the extensions.

 

Rgds,

Laurent

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.